Hello,
I am using custom board, and having some strange behaviour.
It is based on OMAP3530 2.6.37 TI's SDK.
Usb is configured as OTG,
I tried to connect flash device to the board, and I get the following:
[ 2.905609] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 2.913024] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 2
[ 2.921478] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.928649] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.937469] usb usb2: Product: MUSB HDRC host driver
[ 2.942749] usb usb2: Manufacturer: Linux Elbit version 1.6 2.6.37 musb-hcd
[ 2.950103] usb usb2: SerialNumber: musb-hdrc.0
[ 2.958099] hub 2-0:1.0: USB hub found
[ 2.962219] hub 2-0:1.0: 1 port detected
[ 2.969665] i2c /dev entries driver
[ 2.977020] Linux media interface: v0.10
[ 2.982147] lirc_dev: IR Remote Control driver registered, major 250
The usb is detected but there is no sd attached to it, and there is no /dev/sd*
I also see that when I remove and insert the flash memory, it is not detected any more.
Is there any idea what can cause this ? Is it come HW failure behaviour ?
Thank you!
Ran