I've downloaded ipc_3_36_02_13 and have configured products.mak to the best of my ability and have tried to kick off a build with make -f ipc-linux.mak config but autotools isn't happy about a few things so I'm wondering if anyone else has ran into similar issues.
Since DM816x isn't officially supported, I picked the OMAP54XX for platform.
Here is basically what I'm seeing:
hutch@Strider:~/ipc_3_36_02_13$ make -f ipc-linux.mak config
Configuring Linux Ipc ...
./configure --host=arm-poky-linux-gnueabi \
--prefix=/home/hutch/ipc_3_36_02_13 \
CC=/opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc \
PLATFORM=OMAP54XX \
CMEM_INSTALL_DIR= \
KERNEL_INSTALL_DIR=/home/hutch/linux-4.1-rc2_ti816x/linux \
DRM_PREFIX= \
AF_RPMSG=
configure: WARNING: If you wanted to set the --build type, don't use --host.
If a cross compiler is detected then cross compile mode will be used.
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking for arm-poky-linux-gnueabi-strip... no
checking for strip... strip
checking whether to enable maintainer-specific portions of Makefiles... no
checking build system type... x86_64-unknown-linux
checking host system type... arm-poky-linux-gnueabi
checking for style of include used by make... GNU
checking for arm-poky-linux-gnueabi-gcc... /opt/poky/1.8/sysroots/i686-pokysdk-linux/usr/bin/arm-poky-linux-gnueabi/arm-poky-linux-gnueabi-gcc
checking for C compiler default output file name... configure: error: C compiler cannot create executables
See `config.log' for more details.
make: *** [config] Error 77