Dear Pavel,
Linux Kernel hanging issue fixed. It is working if only enable PHY (SMSC) driver in Menuconfig. The problem because of adding decoder and encoder in Menuconfig. can you mail me how to resolve this issue?
Regards
Balaji
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Balaji,
Balaji Govindarajan said:It is working if only enable PHY (SMSC) driver in Menuconfig.
This should indicate that linux kernel is trying to access this PHY, and when there is no driver for it, it hangs.
Balaji Govindarajan said:The problem because of adding decoder and encoder in Menuconfig.
Could you provide more details about this decoder and encoder? What is the problem you see when add decoder and encoder in Menuconfig? How you add them in menuconfig? Why you add them in menuconfig?
Balaji Govindarajan said:Kernel Issue:
I have added ADV7180 decoder and ADV7343 encoder in Menuconfig.
What issue you have exactly when add ADV7180 and ADV7343 in menuconfig? Do you have ADV7180 and ADV7343 populated in your custom board?
BR
Pavel
Balaji,
Do you need to load your root filesystem from NAND (UBIFS) or from Ethernet (NFS)?
BR
Pavel
Also make sure you are using the latest version of the ti816x dvrrdk linux kernel, available at:
http://arago-project.org/git/projects/?p=linux-dvr-rdk-dm81xx.git;a=shortlog;h=refs/heads/dvrrdk_kernel_int_branch
Have a look also in the below e2e threads:
e2e.ti.com/.../211477
e2e.ti.com/.../208040
e2e.ti.com/.../391494
e2e.ti.com/.../202733
e2e.ti.com/.../341010
e2e.ti.com/.../199867
e2e.ti.com/.../242691
e2e.ti.com/.../292842
e2e.ti.com/.../275459
e2e.ti.com/.../343125
BR
Pavel