Am trying to remove the unwanted scripts in argo base rootfs, could any please provide some explanation if each script present in the /etc/init.d/
Kindly do the needful as early as possible
Many thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Am trying to remove the unwanted scripts in argo base rootfs, could any please provide some explanation if each script present in the /etc/init.d/
Kindly do the needful as early as possible
Many thanks in advance
Hi Srini,
In addition.
Those are the init scripts that are executed during board boot up.
They are responsible for starting different daemons & processes in your system, such as: matrix gui, touch screen calibration, dbus, dropbear, lighttpd, splash screen, busybox, alsa, etc..
Usually each script has a short description at the beginning.
Best Regards,
Yordan
Dear Yordan /Titus
Thanks a lot for your quick inputs
processors.wiki.ti.com/.../Sitara_Linux_Training:_Boot_Time_Reduction
1. W.r.t the file systems optimization the above link says that udev can be replaced with mdev, Could you please let me know how this can be done in arago-base-tisdk-image-am335x-evm in ti sdk 8 (I googled a few but it was bits & pieces) with detailed steps & please let me know is there any harm in using mdev (as in my product, I would be using USB as one of the hot pluggable devices) because I see udev in ti sdk 8 argo-base rootfs, it is taking 10 sec,
2. As am newbie to rootfs I need some brief explanation w.r.t the below scripts, once if I get better understanding, I can try to remove which ever the below is not required in the /etc/init.d/
alignment.sh
banner.sh
bootmisc.sh
checkroot.sh
modutils.sh
mountall.sh
populate-volatile.sh
psplash.sh
read-only-rootfs-hook.sh
urandom
modutils.sh
3. And how to disable the login ie., preventing it to enter the password
4. To reduce the time creation of shell
5. How to build uncompressed kernel Image & load it from EMMC
Kindly do the needful as early as possible
Many Thanks in advance
Dear Titus,
I didn't find anything to udev in rc5.d but I found in rcS.d, I have hereby attached the files in folders of rc5.d & rcS.d
Kindly do the needful as early as possible