Hi, I have question about AM437x QSPI boot. The board is customer board and using Linux SDK v1.00.00.00. My customer are using QSPI boot but the u-boot won't boot. No message are displayed on serial console. They searched the reason and found out that "Global Data(gd)" of u-boot wasn't initialized. And they refered to "flags"of gd which was not initialized by using serial driver and found out that the data abort exception was occuring. They took the following workaround and confirmed that it became able to boot from QSPI. <Workaround> They add the process which clears gd area to zero at the top of s_init() in u-boot. I can't find this issue in the following release note of U-boot but is this known issue in SDK v1.00.00.00? processors.wiki.ti.com/.../ If yes, is this issue been fixed in the Newest SDK v2.00.00.00? By the way, when the customer was using SDK v7.01.00.00 this issued didn't occured and QSPI boot was running fine. best regards, g.f.