Hi,
Our product uses the usb for console login.
1. plug usb cable and then open ttyGS0 --> OK
2. open ttyGS0 and then plug usb cable --> nothing can be read from ttyGS0
I am not sure if this is normal for using serial gadget.
Is there any way to test if the cable is plugged or not?
This could help me to add code to reopen ttyGS0.
Thanks.
** AM335x SDK V1.00.00