This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failed to load module: /usr/lib/weston/wayland-backend.so

Hi,

We are working on the am57xx-evm, we are facing the following problem.

root@am57xx-evm:/usr/bin# weston
Date: 2015-10-07 UTC
[21:53:23.754] weston 1.6.0
               wayland.freedesktop.org/
               Bug reports to: bugs.freedesktop.org/enter_bug.cgi
               Build: 1.5.93-5-g2858cc2 configure.ac: bump version to 1.6.0 (2014-09-19 13:40:14 +0300)
[21:53:23.754] OS: Linux, 4.1.6-g52c4aa7, #1 SMP PREEMPT Wed Oct 7 14:52:06 EDT 2015, armv7l
[21:53:23.755] Using config file '/etc//weston.ini'
[21:53:23.755] Loading module '/usr/lib/weston/wayland-backend.so'
[21:53:23.755] Failed to load module: /usr/lib/weston/wayland-backend.so: cannot open shared object file: No such file or directory

Kindly suggest what might be the problem.

Thanks & Regards,

N.V.Subbaiah.