Next USB question.
I have one USB flash drive where the activity light is always flashing after I insert it.
The kernel / filesystem is based on ti-processor-sdk-linux-am335x-evm-01.00.00.00 and tisdk-rootfs-image-am335x-evm.
On a BeagleBone Black, I need to manually mount the drive, but it does not flash unless an I/O operation is active on the drive.
On our board I can get the activity light to stop flashing if I enter a command like "hdparm /dev/sda" even though the command returns an error "HDIO_DRIVE_COMMAND(identify) failed: Invalid argument". If I then try to read a file from the drive the read is successful but the activity light resumes flashing forever.
Any idea on how I can correct this behavior?
Thanks,
Peter Steinberg