Is it possible to stream an ip camera using gstreamer ?
BR
Ammar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Here is few examples:
- capture via v4l2 capture drive->encode->send it via udp
gst-launch v4l2src device=/dev/video0 always-copy=false queue-size=6 ! video/x-raw-yuv-strided, format=(fourcc)NV12, framerate=(fraction)30/1, width=(int)1280, height=(int)720 ! omxbufferalloc numBuffers=6 ! omx_h264enc force-idr=true force-idr-period=25 i-period=0 bitrate=8000000 ! queue ! rtph264pay ! udpsink host=192.168.1.2 ttl-mc=32 port=5004
-send it via udp.
gst-launch -v filesrc location=/home/users/mgashova/Desktop/ff_2.ts typefind=true ! mpegtsdemux ! h264parse ! gstperf ! udpsink host=192.168.1.2
-receive via udp->decode->display
gst-launch udpsrc port=1234 ! queue ! mpegtsdemux ! h264parse ! omx_h264dec ! omx_scaler ! omx_ctrl display-mode=OMX_DC_MODE_1080P_60 ! omx_videosink sync=true
What is the software release that you are using here?
Is it IPNC? If yes the IPNC does not support gstreamer.
Here is the link with examples only for DM81x with gst omx elements.
BR
Margarita