I am using Cypress v2.19 resistive touch controller which is too old for EETI to support. So I was not able to run the Software
After contacting egalax they provided a solution to use usbtouchscreen inbox usb touch screen driver with TSLIB tool to implement calibration.
I downloaded tslib from following location: I followed the following steps: 1./configure 2.make 3.make install
There were no error messages, the library was build successfully.When i try to run the follwing in test folder: ts_print, It gives error of tslib: Selected device is not a touchscreen. On doing #lsusb command it gives output as:
Bus 002 Device 006: ID 0eef:0001 D-WAV Scientific Co., Ltd eGalax Touchscreen.
I had referred other post where it has been mentioned to enter export certain variable in /usr/local/etc/ts.conf file but it gives me error message as segmentation fault.
Similarly i am getting error message when i try to run other program.
Please help.