Hi,
Can anyone help me to implement the Capture writeback scheme in the DM8168 with the EzSDK.
I am using the HDVPSS 01_00_01_44. But the source code seems not having the capture writeback support as I didnt find any "vpsdrv_captureWrbk.c". The DVR_RDK (hdvpss-01_00_01_37) is having this file. Do I need to add this file to the ezsdk for enabling the writeback?
Which drvid/instanceId I should use to enable the Writeback?
Thanks
Sanju