Hi,
I am trying to run the setup.sh script, which I get from "processor SDK Linux Getting Started Guide step 4" to set up NFS and TFTP for beaglebone black board, in order that beaglebone black boots from TFTP and NFS on the host. The whole setup process looks no errors, besides the setup script asks to select kernel images in /tftproot, I expect to see zImage, but it provides zImage-am3w35x-evm.bin instead (I manually copy zImage to /tftproot). After the setup is completed, I don't see the target file system mounted on the host. I have tried number of times, but still get the same failure.
Any help will be appreciated.