hello everybody:
I have a factory board that boots from the MMC0 interface on the AM3354.
U-BOOT version uboot-2014-07 from ti.
Power IC: TPS65217C.
I know that the GP EVM, IDK and EVM SK use a TPS65910 PMIC. But here is as not what influence.
I format card as FAT32 FS and copy MLO and u-boot.img to it, and I set boot pins in 11001b state.
SD card is partitioned into 2 partitions.
- boot partition : MLO , u-boot.img.
- rootfs partition : nothing.
SD card boot the following figure:
it stop at line 16.
when i use u-boot-2-11.09 and sd card boot is normal.
I guess that the spl file(MLO) should load to SRAM and u-boot.img load to DRAM.
By the way, I not use dtb file and i not modified am335x_evm.h file.
Why will go wrong at line 4 and line 13 to 16 .
I am trying to fix the problem, but I have no idea Where to start ?
Hope you can give me advice.