Hi All,
we have am3352 custom board.But we compiled kernel and u-boot with ti yocto setup.and also latest sdk for ti-processors v3.0.0.0xx source.
But our custom board ddr is MT41J128M16JT-125,micro sdcard also same as am335x-evm board,uart0 is evm debug uart. In our Board debug uart connected uarto test points given.those points only we connected RX,Tx pins .But we cant able to get logs on minicom.
we checked processor to mmc0 both evm and custom board .But in custom board while u-boot and kernel loading time we observe mmc data on cro.ie is also milli or nano seconds.In custom board we cant get that issue.
pmic also same compare to evm and custom board.
Is it necessary to add any support in u-boot for custom board? we need to boot the custom board.
can you any body face this issue.please explain whats the problem.
Thanks & Regards
veeranjaneyulu