Dear SIr,
I have alredy posted to TI Wi fi community but still i am facing the problem which is as follows.
i am trying to use the command "git clone git//git.ti.com/wilink8-wlan/build-utilities.git" but i got the error
fatal error:unable to connect git.ti.com:
git.ti.com[0: 198:47.29.151] error = conection refused
could you please help me to solve this error.In mine college campus if i need to access the internet then we have to use the manual proxy setting in our firefox or chome browser that i have already done and since last two years and everyday i can access internet(still today). But with those setting above command is not working. From some post on the TI wifi community i heard that git.ti.com will not work with proxy. If this the case please tell me how to use above git clone command. Here i am inserting the file to have a look on the mannual proxy setting and also i have made it applicable system wide.
Regards
Aditya