Hi there, I am trying to understand how to run applications on the arm core of OMAP-L138.
I have an eval OMAP-L138 LCDK with the Montavista and I would like to know, how can I run some application .
Regards,
Mitesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
should the bootcmd be just uImage ? or should it be the full uImage*.bin ?
Loading T T T T .....
Retry count exceeded; starting again
Hi Shankari,
there were few problems with the commands...
1) The file name in /tftpboot/uImage was not uImage! it was uImage-omapl138-lcdk.bin
2) the u-boot env bootargs value for console=/dev/ttyS2 should have been console=/dev/ttyUSB0
To verify that the ARM is boot linux from linux host can I removed the SD card and reboot?
Hi Shankari,
Yeah, thats true. I had to copy u-boot_omapl138.bin to uImage in /tftpboot/ I guess it was created when running the setup script, provided with the MCSDK.
And about the ttyS2, yeah your are right.
Lastly, when I tried to remove the SD card and reboot the lcdk it didn't work. It just doesn't reboot without SD card.
And for some reason, I am not able to use my Linux host machine any more. It just keeps restarting. (Doesn't restart completely but keeps locking the screen and closing all the apps)
Hi
I am manged to get the MCSDK 1.01.00.02 on Ubuntu 16.4
I also got the tftp server running and I can see the LCDK booting up from the targerFS... (from linux host )
But It looks like I will have to have the u-boot in the Nand flash for it to work..
could you please tell me how can I rebuild u-boot or how can I flash default u-boot if provided with the mcsdk. thanks.
Thanks Shankari, now back to the original question.
I would like to install or run web server from the arm processor (ARM core on the OMAPL138)
should I install PHP and Apache on the Target Linux or Host Linux PC?
Or do I need to have a cross compiler similar to arago-linux-gnueabi -gcc ?
thanks .