Hi all ,
We are trying to modify the CPSW setting to forward all received traffic from external ports to the host port. Currently Board ethernet interface receives the traffic if the destination MAC is board's MAC address, remaining packets are dropped at the inteface level itself (Not even traced by tcpdump).
- We need to set the Bypass flag to 1 in ALE_CONTROL to achieve the above requirement . But we were not able to modify the bypass flag value in ALE_CONTROL, even editing using "vi" was not helpful - change was not reflected in the Ale_control . How to change the ALE_CONTROL values in ARM ?
- Commands tried :
- echo "bypass=1" > cat /sys/devices/soc6614.0/2090000.netcp/ale_control
- echo "bypass=1" >cat /sys/class/net/eth0/device/ale_control
Not able to modify the Ale_control values . Is it read/Write protected ?
Linux Kernel : Arago linux-3.4.40.
regards ,
vinodh