Hello,
I have an issue with omap,
I am working with fpga, which implements mac.
communicating with fpga is through gpmc.
It works well, until I get the following lines:
[ 69.317016] do_calibrate: core: Calibration complete: Voltage Nominal=962000Calib=848260 margin=38000
[ 69.317169] do_calibrate: mpu: Calibration complete: Voltage Nominal=1025000Calib=800000 margin=10000
After that I can still access fpga, but not mac address.
Does anyone knows what these lines means ?
Regards,
Ran