Tool/software: Linux
Hello TI,
We have a custom board mostly based on the Beaglebone Black. I have been struggling mightily to mux 3 pins as gpios (simple right?) and I am unable to make that happen. The un-muxable pins are:
- gpio0_1 (pin 83 (44e1094c.0)) ,
- gpio2_21 (pin 80 (44e10940.0)), and
- gpio3_18 (pin 104 (44e109a0.0)).
I am sure (famous last words) that my device tree is properly programmed, and I can include the fdtdump that shows that the pins reassigned as gpios if you want. But when I look at '/sys/kernel/debug/pinctrl/44e10800.pinmux.pins', it says
- gpio0_1 never changed out of mode 0,
- gpio2_21 never changed out of mode 0, and
- gpio3_18 never changed out of mode 4.
Any advice *greatly* appreciated. Thank you.
Scott