Tool/software: Linux
Hi all,
I am using OMAP L138 LCDK with Linux OS. I have compiled and loaded Linux kernel version 3.3 after configuring with the below command.
$sudo make da850_lcdk_defconfig ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi-
My board is booting and working properly.
Now I want to work on ALSA. The LCDK has two capture ports as Line In and Mic. I have given alsa device list command and its output below.
root@omapl138-lcdk:~# arecord -L
null
Discard all samples (playback) or generate zero samples (capture)
default:CARD=EVM
DA850/OMAP-L138 EVM,
Default Audio Device
sysdefault:CARD=EVM
DA850/OMAP-L138 EVM,
Default Audio Device
I can capture audio from Line In port easily using arecord commands. But I want to capture audio from Mic input. I have connected a standard 3.5 mm single channel laptop microphone to Mic port. No sound is getting captured. I don't know what mistake I have done. Kindly help me.
Thanks in advanced....
Regards,
Jagadish Haldar