Tool/software: Linux
Hi,
We have developed a custom board with AM5718 processor and we are using ti-processor-sdk-linux-am57xx-evm-02.00.01.07. I am using eMMC boot mode and please check the bootlog in which we are getting error with CMEMK and also it takes 3 seconds for initialization of USB. Please help me in this regard.
U-Boot SPL 2015.07-00080-g4523775-dirty (Feb 03 2017 - 14:37:54)
DRA722 ES1.0
U-Boot SPL 2015.07-00080-g4523775-dirty (Feb 03 2017 - 14:37:54)
DRA722 ES1.0
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
ti_i2c_eeprom_init failed 1
U-Boot 2015.07-00080-g4523775-dirty (Feb 03 2017 - 14:37:54 +0530)
CPU : DRA722 ES1.0
Board: AM571x II2C: ready
DRAM: 1 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
**********Auto Negotiation Available******cpsw
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
Card did not respond to voltage select!
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
reading uEnv.txt
574 bytes read in 5 ms (111.3 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc1 ...
3372440 bytes read in 211 ms (15.2 MiB/s)
85517 bytes read in 41 ms (2 MiB/s)
Booting from mmc1 ...
Card did not respond to voltage select!
** Bad device mmc 0 **
Kernel image @ 0x82000000 [ 0x000000 - 0x337598 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe8000, end 8ffffe0c ... OK
Starting Medha kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.1.13-g8dc6617 (medha@medha) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #33 SMP PREEMPT7
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI AM571x IDK
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] DRA722 ES1.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @eee50000 s16128 r8192 d20736 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 210514
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=6750ca45-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 650204K/848896K available (6315K kernel code, 291K rwdata, 2188K rodata, 332K init, 254K bss, 18468K reserved, 180224K )
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xef800000 ( 760 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0856074 (8505 kB)
[ 0.000000] .init : 0xc0857000 - 0xc08aa000 ( 332 kB)
[ 0.000000] .data : 0xc08aa000 - 0xc08f2f88 ( 292 kB)
[ 0.000000] .bss : 0xc08f5000 - 0xc093480c ( 255 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] OMAP clockevent source: timer1 at 32768 Hz
[ 0.000000] clocksource 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000030] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[ 0.000030] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000427] Architected cp15 timer(s) running at 6.14MHz (virt).
[ 0.000427] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000462] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000472] Switching to timer-based delay loop, resolution 162ns
[ 0.000962] Console: colour dummy device 80x30
[ 0.000977] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000983] This ensures that you still see kernel messages. Please
[ 0.000988] update your kernel commandline.
[ 0.001000] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.001012] pid_max: default: 32768 minimum: 301
[ 0.001095] Security Framework initialized
[ 0.001131] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001141] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001662] Initializing cgroup subsys blkio
[ 0.001677] Initializing cgroup subsys memory
[ 0.001703] Initializing cgroup subsys devices
[ 0.001715] Initializing cgroup subsys freezer
[ 0.001726] Initializing cgroup subsys perf_event
[ 0.001747] CPU: Testing write buffer coherency: ok
[ 0.002003] /cpus/cpu@0 missing clock-frequency property
[ 0.002015] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002046] Setting up static identity map for 0x80008380 - 0x800083d8
[ 0.040749] Brought up 1 CPUs
[ 0.040761] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[ 0.040768] CPU: All CPU(s) started in SVC mode.
[ 0.041120] devtmpfs: initialized
[ 0.063648] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.064440] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.077136] omap_hwmod: tptc0 using broken dt data from edma-controller
[ 0.077588] omap_hwmod: tptc1 using broken dt data from edma-controller
[ 0.151051] omap_hwmod: dcan2: _wait_target_disable failed
[ 0.251631] omap_hwmod: rtcss: _wait_target_disable failed
[ 0.251641] omap_hwmod: rtcss: _wait_target_ready failed: -16
[ 0.251651] omap_hwmod: rtcss: cannot be enabled for reset (3)
[ 0.253142] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.256972] pinctrl core: initialized pinctrl subsystem
[ 0.257219] Regulator Name : regulator-dummy
[ 0.257333] Regulator Name : regulator-dummy added
[ 0.257771] NET: Registered protocol family 16
[ 0.258686] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.266762] OMAP GPIO hardware version 0.1
[ 0.289741] No ATAGs?
[ 0.289765] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.289774] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.292232] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.292242] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.292801] OMAP DMA hardware revision 0.0
[ 0.327962] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[ 0.330621] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[ 0.331095] Regulator Name : evm_3v3_sd
[ 0.331225] Regulator Name : evm_3v3_sd added
[ 0.331366] Regulator Name : vtt_fixed
[ 0.331530] Regulator Name : vtt_fixed added
[ 0.334773] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.334946] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.335108] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.335262] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.335517] vgaarb: loaded
[ 0.335877] SCSI subsystem initialized
[ 0.337402] palmas 0-0058: IRQ missing: skipping irq request
[ 0.351068] palmas 0-0058: Muxing GPIO 51, PWM 0, LED 2
[ 0.352321] Regulator Name : SMPS1
[ 0.352948] Regulator Name : SMPS1 added
[ 0.353581] Regulator Name : SMPS2
[ 0.354198] Regulator Name : SMPS2 added
[ 0.354815] Regulator Name : SMPS3
[ 0.355432] Regulator Name : SMPS3 added
[ 0.356048] Regulator Name : SMPS4
[ 0.356663] Regulator Name : SMPS4 added
[ 0.357287] Regulator Name : SMPS5
[ 0.357900] Regulator Name : SMPS5 added
[ 0.357936] Regulator Name : LDO1
[ 0.360757] Regulator Name : LDO1 added
[ 0.361075] Regulator Name : LDO2
[ 0.361524] Regulator Name : LDO2 added
[ 0.361836] Regulator Name : LDO3
[ 0.370773] Regulator Name : LDO3 added
[ 0.371081] Regulator Name : LDO4
[ 0.380789] Regulator Name : LDO4 added
[ 0.381102] Regulator Name : LDO5
[ 0.390805] Regulator Name : LDO5 added
[ 0.391118] Regulator Name : REGEN1
[ 0.391223] Regulator Name : REGEN1 added
[ 0.391259] Regulator Name : REGEN2
[ 0.391365] Regulator Name : REGEN2 added
[ 0.391409] Regulator Name : REGEN3
[ 0.391515] Regulator Name : REGEN3 added
[ 0.391577] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.391740] media: Linux media interface: v0.10
[ 0.391796] Linux video capture interface: v2.00
[ 0.391839] pps_core: LinuxPPS API ver. 1 registered
[ 0.391846] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.391871] PTP clock support registered
[ 0.392505] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[ 0.392790] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[ 0.393059] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.393128] omap-mailbox: probe of 48842000.mailbox failed with error -22
[ 0.393342] Advanced Linux Sound Architecture Driver Initialized.
[ 0.393973] Switched to clocksource arch_sys_counter
[ 0.403595] NET: Registered protocol family 2
[ 0.404185] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.404249] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.404374] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.404428] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.404459] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.404663] NET: Registered protocol family 1
[ 0.404903] RPC: Registered named UNIX socket transport module.
[ 0.404912] RPC: Registered udp transport module.
[ 0.404918] RPC: Registered tcp transport module.
[ 0.404924] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.405848] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[ 0.405877] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.407721] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.407792] audit: initializing netlink subsys (disabled)
[ 0.407827] audit: type=2000 audit(0.390:1): initialized
[ 0.414791] VFS: Disk quotas dquot_6.6.0
[ 0.414947] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.416900] NFS: Registering the id_resolver key type
[ 0.416931] Key type id_resolver registered
[ 0.416938] Key type id_legacy registered
[ 0.416992] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.419339] NET: Registered protocol family 38
[ 0.419417] bounce: pool size: 64 pages
[ 0.419432] io scheduler noop registered
[ 0.419444] io scheduler deadline registered
[ 0.419483] io scheduler cfq registered (default)
[ 0.421598] Device Name is 4a096000.phy
[ 0.421607] has_full_constraints = 0
[ 0.421613] of_have_populated_dt() = 1
[ 0.421620] Looking up phy-supply from device tree
[ 0.421626] Looking up phy-supply-prop_name from device tree
[ 0.421635] Looking up phy-supply property in node /ocp/ocp2scp@4a090000/phy@4A096000 failed
[ 0.421646] has_full_constraints = 0
[ 0.421652] of_have_populated_dt() = 1
[ 0.421657] has_full_constraints = 0
[ 0.421662] of_have_populated_dt() = 1
[ 0.422075] Device Name is 4a094000.pciephy
[ 0.422083] has_full_constraints = 0
[ 0.422089] of_have_populated_dt() = 1
[ 0.422095] Looking up phy-supply from device tree
[ 0.422101] Looking up phy-supply-prop_name from device tree
[ 0.422109] Looking up phy-supply property in node /ocp/ocp2scp@4a090000/pciephy@4a094000 failed
[ 0.422116] has_full_constraints = 0
[ 0.422122] of_have_populated_dt() = 1
[ 0.422127] has_full_constraints = 0
[ 0.422132] of_have_populated_dt() = 1
[ 0.422381] Device Name is 4a084400.phy
[ 0.422388] has_full_constraints = 0
[ 0.422394] of_have_populated_dt() = 1
[ 0.422400] Looking up phy-supply from device tree
[ 0.422407] Looking up phy-supply-prop_name from device tree
[ 0.422414] Looking up phy-supply property in node /ocp/ocp2scp@4a080000/phy@4a084400 failed
[ 0.422421] has_full_constraints = 0
[ 0.422427] of_have_populated_dt() = 1
[ 0.422432] has_full_constraints = 0
[ 0.422437] of_have_populated_dt() = 1
[ 0.423049] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[ 0.423161] pinctrl-single 4a002e8c.pinmux: 1 pins at pa fc002e8c size 4
[ 0.456088] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[ 0.456100] pci_bus 0000:00: root bus resource [io 0x1000-0xffff]
[ 0.456111] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.456122] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.456242] pci 0000:00:00.0: IOMMU is currently not supported for PCI
[ 0.456521] PCI: bus0: Fast back to back transfers disabled
[ 0.456642] PCI: bus1: Fast back to back transfers enabled
[ 0.456736] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.456751] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.456763] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.458385] Device Name is 58000000.dss
[ 0.458393] has_full_constraints = 0
[ 0.458399] of_have_populated_dt() = 1
[ 0.458406] Looking up vdda_video-supply from device tree
[ 0.458412] Looking up vdda_video-supply-prop_name from device tree
[ 0.458439] Looking up ldo5-in-supply from device tree
[ 0.458446] Looking up ldo5-in-supply-prop_name from device tree
[ 0.458452] Looking up ldo5-in-supply property in node /ocp/i2c@48070000/tps65917@58/tps65917_pmic failed
[ 0.458793] OMAP DSS rev 6.1
[ 0.459060] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[ 0.474073] tlc59108 0-0040: Successfully initialized tlc59108
[ 0.474386] Regulator Name : pbias_mmc_omap5
[ 0.474529] Regulator Name : pbias_mmc_omap5 added
[ 0.474974] Regulator Name : 4ae07ddc.regulator-abb-mpu
[ 0.475109] Regulator Name : 4ae07ddc.regulator-abb-mpu added
[ 0.475259] Regulator Name : 4ae07e34.regulator-abb-ivahd
[ 0.475387] Regulator Name : 4ae07e34.regulator-abb-ivahd added
[ 0.475532] Regulator Name : 4ae07e30.regulator-abb-dspeve
[ 0.475664] Regulator Name : 4ae07e30.regulator-abb-dspeve added
[ 0.475816] Regulator Name : 4ae07de4.regulator-abb-gpu
[ 0.475942] Regulator Name : 4ae07de4.regulator-abb-gpu added
[ 0.476569] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[ 0.479429] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 299, base_baud = 3000000) is a 8250
[ 1.778488] console [ttyS0] enabled
[ 1.782954] [drm] Initialized drm 1.1.0 20060810
[ 1.795818] brd: module loaded
[ 1.802877] loop: module loaded
[ 1.806961] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 1.814805] libphy: Fixed MDIO Bus: probed
[ 1.863991] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.870115] davinci_mdio 48485000.mdio: detected phy mask fffffdff
[ 1.878366] libphy: 48485000.mdio: probed
[ 1.882395] davinci_mdio 48485000.mdio: phy[9]: device 48485000.mdio:09, driver unknown
[ 1.890997] cpsw 48484000.ethernet: Missing slave[1] phy_id property
[ 1.897430] cpsw 48484000.ethernet: Detected MACID = 74:da:ea:0c:dc:a2
[ 1.905511] mousedev: PS/2 mouse device common for all mice
[ 1.911165] i2c /dev entries driver
[ 1.915603] tmp102 0-0048: error reading config register
[ 1.920947] tmp102: probe of 0-0048 failed with error -121
[ 1.927690] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.932552] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr104 mode
[ 1.939070] omap_hsmmc 4809c000.mmc: no pinctrl state for ddr50 mode
[ 1.945468] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr50 mode
[ 1.951850] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr25 mode
[ 1.958246] omap_hsmmc 4809c000.mmc: no pinctrl state for sdr12 mode
[ 1.964641] omap_hsmmc 4809c000.mmc: no pinctrl state for hs mode
[ 1.970925] Device Name is 4809c000.mmc
[ 1.974968] has_full_constraints = 0
[ 1.978643] of_have_populated_dt() = 1
[ 1.982494] Looking up vmmc-supply from device tree
[ 1.987580] Looking up vmmc-supply-prop_name from device tree
[ 1.993605] Device Name is 4809c000.mmc
[ 1.997647] has_full_constraints = 0
[ 2.001320] of_have_populated_dt() = 1
[ 2.005187] Looking up vmmc_aux-supply from device tree
[ 2.010608] Looking up vmmc_aux-supply-prop_name from device tree
[ 2.016916] Looking up vmmc_aux-supply property in node /ocp/mmc@4809c000 failed
[ 2.024184] has_full_constraints = 0
[ 2.028039] of_have_populated_dt() = 1
[ 2.031888] has_full_constraints = 0
[ 2.035576] of_have_populated_dt() = 1
[ 2.039427] Device Name is 4809c000.mmc
[ 2.043451] has_full_constraints = 0
[ 2.047180] of_have_populated_dt() = 1
[ 2.051030] Looking up pbias-supply from device tree
[ 2.056205] Looking up pbias-supply-prop_name from device tree
[ 2.094626] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.102068] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.110501] omap_hsmmc 480b4000.mmc: no pinctrl state for ddr_1_8v mode
[ 2.117209] omap_hsmmc 480b4000.mmc: no pinctrl state for hs mode
[ 2.123377] omap_hsmmc 480b4000.mmc: no pinctrl state for hs200_1_8v mode
[ 2.130416] Device Name is 480b4000.mmc
[ 2.134506] has_full_constraints = 0
[ 2.138229] of_have_populated_dt() = 1
[ 2.142124] Looking up vmmc-supply from device tree
[ 2.147256] Looking up vmmc-supply-prop_name from device tree
[ 2.153324] Device Name is 480b4000.mmc
[ 2.157419] has_full_constraints = 0
[ 2.162163] of_have_populated_dt() = 1
[ 2.166030] Looking up vmmc_aux-supply from device tree
[ 2.171450] Looking up vmmc_aux-supply-prop_name from device tree
[ 2.177756] Looking up vmmc_aux-supply property in node /ocp/mmc@480b4000 failed
[ 2.185023] has_full_constraints = 0
[ 2.188878] of_have_populated_dt() = 1
[ 2.192726] has_full_constraints = 0
[ 2.196414] of_have_populated_dt() = 1
[ 2.200264] Device Name is 480b4000.mmc
[ 2.204301] has_full_constraints = 0
[ 2.207975] of_have_populated_dt() = 1
[ 2.211822] Looking up pbias-supply from device tree
[ 2.216993] Looking up pbias-supply-prop_name from device tree
[ 2.223024] Looking up pbias-supply property in node /ocp/mmc@480b4000 failed
[ 2.230028] has_full_constraints = 0
[ 2.233883] of_have_populated_dt() = 1
[ 2.237745] has_full_constraints = 0
[ 2.241418] of_have_populated_dt() = 1
[ 2.284243] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.290617] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[ 2.300280] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[ 2.306635] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[ 2.313523] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[ 2.323812] oprofile: using timer interrupt.
[ 2.330444] Initializing XFRM netlink socket
[ 2.334836] NET: Registered protocol family 17
[ 2.339325] NET: Registered protocol family 15
[ 2.343857] Key type dns_resolver registered
[ 2.348365] omap_voltage_late_init: Voltage driver support not added
[ 2.355054] Power Management for TI OMAP4+ devices.
[ 2.360198] ThumbEE CPU extension supported.
[ 2.364569] Registering SWP/SWPB emulation handler
[ 2.370914] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.378424] dmm 4e000000.dmm: initialized all PAT entries
[ 2.383879] mmc1: MAN_BKOPS_EN bit is not set
[ 2.389218] mmc1: new MMC card at address 0001
[ 2.394042] mmcblk0: mmc1:0001 MMC04G 3.60 GiB
[ 2.398704] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
[ 2.406368] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 2.413013] [drm] No driver support for vblank timestamp query.
[ 2.419158] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
[ 2.428345] mmcblk0: p1 p2
[ 2.432443] [drm] Enabling DMM ywrap scrolling
[ 2.477646] Console: switching to colour frame buffer device 100x37
[ 2.487398] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[ 2.493343] omapdrm omapdrm.0: registered panic notifier
[ 2.524170] omapwb-m2m: Device registered as video10
[ 2.529158] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[ 2.535503] hctosys: unable to open rtc device (rtc0)
[ 2.552460] has_full_constraints = 1
[ 2.556167] of_have_populated_dt() = 1
[ 2.560017] ldo4: disabling
[ 2.563504] ALSA device list:
[ 2.566502] No soundcards found.
[ 2.680643] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 2.688842] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.703445] devtmpfs: mounted
[ 2.706654] Freeing unused kernel memory: 332K (c0857000 - c08aa000)
INIT: version 2.88 booting
Starting udev
[ 5.709459] udevd[96]: starting version 182
[ 6.590404] extcon-usb-gpio extcon_usb1: failed to get ID GPIO
[ 6.672698] extcon-usb-gpio: probe of extcon_usb1 failed with error -2
[ 6.791806] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[ 7.082388] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[ 7.114374] vpe 489d0000.vpe: Device registered as /dev/video0
[ 7.180214] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 8.157466] Device Name is 4a084000.phy
[ 8.220432] has_full_constraints = 1
[ 8.273565] of_have_populated_dt() = 1
[ 8.277496] Looking up phy-supply from device tree
[ 8.282488] Looking up phy-supply-prop_name from device tree
[ 8.288466] Looking up ldo4-in-supply from device tree
[ 8.293807] Looking up ldo4-in-supply-prop_name from device tree
[ 8.300125] Looking up ldo4-in-supply property in node /ocp/i2c@48070000/tps65917@58/tps65917_pmic failed
[ 8.311264] Device Name is 4a085000.phy
[ 8.315543] has_full_constraints = 1
[ 8.319227] of_have_populated_dt() = 1
[ 8.323081] Looking up phy-supply from device tree
[ 8.328108] Looking up phy-supply-prop_name from device tree
[ 8.334007] Looking up ldo4-in-supply from device tree
[ 8.339345] Looking up ldo4-in-supply-prop_name from device tree
[ 8.345570] Looking up ldo4-in-supply property in node /ocp/i2c@48070000/tps65917@58/tps65917_pmic failed
/************************************3 seconds waiting time here*********************************************************************/
[ 11.622579] usbcore: registered new interface driver usbfs
[ 11.630277] usbcore: registered new interface driver hub
[ 11.636399] usbcore: registered new device driver usb
[ 12.134706] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 12.140445] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 12.148679] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[ 12.157662] xhci-hcd xhci-hcd.0.auto: irq 415, io mem 0x488d0000
[ 12.164044] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 12.171002] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.178407] usb usb1: Product: xHCI Host Controller
[ 12.183434] usb usb1: Manufacturer: Linux 4.1.13-g8dc6617 xhci-hcd
[ 12.189783] usb usb1: SerialNumber: xhci-hcd.0.auto
[ 12.195644] hub 1-0:1.0: USB hub found
[ 12.199592] hub 1-0:1.0: 1 port detected
[ 12.204949] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 12.210646] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 12.218615] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 12.227033] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[ 12.234054] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 12.241456] usb usb2: Product: xHCI Host Controller
[ 12.246508] usb usb2: Manufacturer: Linux 4.1.13-g8dc6617 xhci-hcd
[ 12.252843] usb usb2: SerialNumber: xhci-hcd.0.auto
[ 12.258972] hub 2-0:1.0: USB hub found
[ 12.262777] hub 2-0:1.0: 1 port detected
[ 12.514046] usb 1-1: new full-speed USB device number 2 using xhci-hcd
[ 12.672642] usb 1-1: New USB device found, idVendor=03eb, idProduct=212c
[ 12.679398] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 12.686580] usb 1-1: Product: Atmel maXTouch Digitizer
[ 12.691741] usb 1-1: Manufacturer: Atmel
[ 13.069232] input: Atmel Atmel maXTouch Digitizer as /devices/platform/44000000.ocp/488c0000.omap_dwc3_2/488d0000.usb/xhci-hcd.0.auto/usb1/0
[ 13.086932] hid-multitouch 0003:03EB:212C.0001: input,hiddev0: USB HID v1.11 Device [Atmel Atmel maXTouch Digitizer] on usb-xhci-hcd.0.auto0
[ 13.107011] hid-generic 0003:03EB:212C.0002: hiddev0: USB HID v1.11 Device [Atmel Atmel maXTouch Digitizer] on usb-xhci-hcd.0.auto-1/input1
[ 13.121203] usbcore: registered new interface driver usbhid
[ 13.127021] usbhid: USB HID core driver
[ 13.176711] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[ 13.240266] Error: Driver 'hid-generic' is already registered, aborting...
[ 13.274431] Error: Driver 'hid-multitouch' is already registered, aborting...
/*****************************Kernel panic with CMEMK module****************************************************/
[ 13.866414] CMEMK module: reference Linux version 4.1.13
[ 13.874118] allocated heap buffer 0x40500000 of size 0x100000
[ 13.879923] ------------[ cut here ]------------
[ 13.884569] WARNING: CPU: 0 PID: 537 at drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x248/0x34c()
[ 13.894090] 44000000.ocp:L3 Standard Error: MASTER MPU TARGET OCMC_RAM3 (Read Link): At Address: 0x00000000 : Data Access in User mode duris
[ 13.908403] Modules linked in: cmemk(O+) evdev joydev usbhid xhci_plat_hcd xhci_hcd usbcore dwc3 omapdrm_pvr(O) udc_core phy_omap_usb2 omapn
[ 13.928994] CPU: 0 PID: 537 Comm: modprobe Tainted: G O 4.1.13-g8dc6617 #33
[ 13.937117] Hardware name: Generic DRA72X (Flattened Device Tree)
[ 13.943233] Backtrace:
[ 13.945704] [<c0013018>] (dump_backtrace) from [<c001323c>] (show_stack+0x18/0x1c)
[ 13.953303] r7:c030ff28 r6:00000093 r5:c08c990c r4:00000000
[ 13.959027] [<c0013224>] (show_stack) from [<c0628dfc>] (dump_stack+0x9c/0xdc)
[ 13.966286] [<c0628d60>] (dump_stack) from [<c0039748>] (warn_slowpath_common+0x88/0xb8)
[ 13.974407] r5:00000009 r4:ec52fb80
[ 13.978015] [<c00396c0>] (warn_slowpath_common) from [<c00397b0>] (warn_slowpath_fmt+0x38/0x40)
[ 13.986747] r8:c07cf674 r7:00000004 r6:ee95af50 r5:c07cf728 r4:c07cf7d8
[ 13.993519] [<c003977c>] (warn_slowpath_fmt) from [<c030ff28>] (l3_interrupt_handler+0x248/0x34c)
[ 14.002424] r3:ee95adc0 r2:c07cf7d8
[ 14.006025] r4:80080001
[ 14.008581] [<c030fce0>] (l3_interrupt_handler) from [<c0079ac4>] (handle_irq_event_percpu+0x80/0x13c)
[ 14.017924] r10:c08f2729 r9:ee941780 r8:00000017 r7:00000000 r6:00000000 r5:ee9417e0
[ 14.025824] r4:ee9602c0
[ 14.028379] [<c0079a44>] (handle_irq_event_percpu) from [<c0079bc4>] (handle_irq_event+0x44/0x64)
[ 14.037286] r10:bf178fc0 r9:bf178cc0 r8:ee806000 r7:00000000 r6:ee9602c0 r5:ee9417e0
[ 14.045184] r4:ee941780
[ 14.047737] [<c0079b80>] (handle_irq_event) from [<c007c8f0>] (handle_fasteoi_irq+0xb8/0x17c)
[ 14.056294] r7:00000000 r6:c08b1a7c r5:ee9417e0 r4:ee941780
[ 14.062009] [<c007c838>] (handle_fasteoi_irq) from [<c0079128>] (generic_handle_irq+0x34/0x44)
[ 14.070654] r7:00000000 r6:00000000 r5:00000017 r4:00000017
[ 14.076372] [<c00790f4>] (generic_handle_irq) from [<c0079400>] (__handle_domain_irq+0x64/0xbc)
[ 14.085103] r5:00000017 r4:c08a6d2c
[ 14.088711] [<c007939c>] (__handle_domain_irq) from [<c00094ac>] (gic_handle_irq+0x2c/0x64)
[ 14.097094] r9:bf178cc0 r8:bf178a40 r7:fa212000 r6:ec52fd30 r5:c08ac950 r4:fa21200c
[ 14.104912] [<c0009480>] (gic_handle_irq) from [<c062ee40>] (__irq_svc+0x40/0x74)
[ 14.112424] Exception stack(0xec52fd30 to 0xec52fd78)
[ 14.117497] fd20: f0ffa000 f0ffb000 bf178fc0 00100000
[ 14.125710] fd40: df5a8540 00000004 40500000 00000000 bf178a40 bf178cc0 bf178fc0 ec52fd84
[ 14.133921] fd60: ec52fd78 ec52fd78 c01030a4 c0102eb8 20030013 ffffffff
[ 14.140560] r7:ec52fd64 r6:ffffffff r5:20030013 r4:c0102eb8
[ 14.146289] [<c0103090>] (unmap_kernel_range_noflush) from [<bf17c41c>] (init_module+0x41c/0x5e4 [cmemk])
[ 14.155905] [<bf17c000>] (init_module [cmemk]) from [<c0009848>] (do_one_initcall+0x94/0x1e0)
[ 14.164463] r10:00000000 r9:edfecd08 r8:1201331c r7:df5a80c0 r6:c08af130 r5:bf17c000
[ 14.172365] r4:c08af130
[ 14.174917] [<c00097b4>] (do_one_initcall) from [<c0626cc0>] (do_init_module+0x64/0x1b0)
[ 14.183038] r10:bf176e84 r9:edfecd08 r8:1201331c r7:00000001 r6:df5a8080 r5:00000001
[ 14.190938] r4:bf176e84
[ 14.193493] [<c0626c5c>] (do_init_module) from [<c00a3298>] (load_module+0x17cc/0x1e10)
[ 14.201527] r6:edfecd00 r5:00000001 r4:ec52ff48
[ 14.206188] [<c00a1acc>] (load_module) from [<c00a3a7c>] (SyS_finit_module+0x6c/0x7c)
[ 14.214048] r10:00000000 r9:ec52e000 r8:c000fba4 r7:0000017b r6:0002ac84 r5:00000003
[ 14.221948] r4:00000000
[ 14.224501] [<c00a3a10>] (SyS_finit_module) from [<c000fa00>] (ret_fast_syscall+0x0/0x3c)
[ 14.232708] r6:00040000 r5:00000000 r4:00000000
[ 14.237364] ---[ end trace 865ce1654477e3d9 ]---
[ 14.242109] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000
[ 14.249448] pgd = ec424600
[ 14.252163] [00000000] *pgd=9f410003, *pmd=9f541003, *pte=00000000
[ 14.258394] Internal error: : 1211 [#1] PREEMPT SMP ARM
[ 14.263637] Modules linked in: cmemk(O+) evdev joydev usbhid xhci_plat_hcd xhci_hcd usbcore dwc3 omapdrm_pvr(O) udc_core phy_omap_usb2 omapn
[ 14.284222] CPU: 0 PID: 537 Comm: modprobe Tainted: G W O 4.1.13-g8dc6617 #33
[ 14.292344] Hardware name: Generic DRA72X (Flattened Device Tree)
[ 14.298461] task: df579e00 ti: ec52e000 task.ti: ec52e000
[ 14.303883] PC is at vunmap_page_range+0x4/0x1a0
[ 14.308519] LR is at unmap_kernel_range_noflush+0x14/0x18
[ 14.313939] pc : [<c0102eb8>] lr : [<c01030a4>] psr: 20030013
[ 14.313939] sp : ec52fd78 ip : ec52fd78 fp : ec52fd84
[ 14.325464] r10: bf178fc0 r9 : bf178cc0 r8 : bf178a40
[ 14.330708] r7 : 00000000 r6 : 40500000 r5 : 00000004 r4 : df5a8540
[ 14.337261] r3 : 00100000 r2 : bf178fc0 r1 : f0ffb000 r0 : f0ffa000
[ 14.343814] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 14.350977] Control: 30c5387d Table: ac424600 DAC: fffffffd
[ 14.356745] Process modprobe (pid: 537, stack limit = 0xec52e218)
[ 14.362860] Stack: (0xec52fd78 to 0xec530000)
[ 14.367234] fd60: ec52fdec ec52fd88
[ 14.375446] fd80: bf17c41c c010309c bf179228 00000000 bf1791f0 00000000 40500000 00000000
[ 14.383657] fda0: c006f880 bf1791f0 bf178958 00000008 bf178fc0 00000001 ec52fde0 f0ffa000
[ 14.391869] fdc0: c02efc60 c08af130 bf17c000 c08af130 df5a80c0 1201331c edfecd08 00000000
[ 14.400080] fde0: ec52fe6c ec52fdf0 c0009848 bf17c00c 00000000 bf176e84 ec52fe44 ef4e0510
[ 14.408293] fe00: ee801e40 ec424380 c0104ad4 ec52e000 ec52fe28 ec52e028 ec52fe5c ec52fe28
[ 14.416504] fe20: c010faf0 c010efa4 00000001 1201331c edfecd08 00000033 ec424380 f210a000
[ 14.424717] fe40: 00000001 bf176e84 00000001 df5a8080 00000001 1201331c edfecd08 bf176e84
[ 14.432928] fe60: ec52fe94 ec52fe70 c0626cc0 c00097c0 ec52fe94 ec52fe80 c0104bc0 ec52ff48
[ 14.441139] fe80: 00000001 edfecd00 ec52ff44 ec52fe98 c00a3298 c0626c68 bf176e90 00007fff
[ 14.449351] fea0: c00a047c c011e5dc 00032765 00000154 00000000 bf176e90 c08ac570 bf179230
[ 14.457564] fec0: bf176fb8 bf176ecc f210a000 00032765 0002cb9d 00000000 0b300002 00000000
[ 14.465775] fee0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 14.473986] ff00: 00000000 00000000 00000000 00000000 00000000 00000000 000001a0 00000000
[ 14.482199] ff20: 00000003 0002ac84 0000017b c000fba4 ec52e000 00000000 ec52ffa4 ec52ff48
[ 14.490410] ff40: c00a3a7c c00a1ad8 f210a000 00032765 f212d50c f212d373 f213b8f4 00006230
[ 14.498621] ff60: 00006f50 00000000 00000000 00000000 0000002c 0000002d 00000016 00000013
[ 14.506833] ff80: 0000000f 00000000 00000000 00000000 00000000 00040000 00000000 ec52ffa8
[ 14.515045] ffa0: c000fa00 c00a3a1c 00000000 00000000 00000003 0002ac84 00000000 00000000
[ 14.523257] ffc0: 00000000 00000000 00040000 0000017b 00000000 0003d398 00000000 0003d1e8
[ 14.531469] ffe0: be8589d8 be8589c8 00020784 b6f1bc52 800f0030 00000003 00000000 00000000
[ 14.539676] Backtrace:
[ 14.542150] [<c0103090>] (unmap_kernel_range_noflush) from [<bf17c41c>] (init_module+0x41c/0x5e4 [cmemk])
[ 14.551766] [<bf17c000>] (init_module [cmemk]) from [<c0009848>] (do_one_initcall+0x94/0x1e0)
[ 14.560325] r10:00000000 r9:edfecd08 r8:1201331c r7:df5a80c0 r6:c08af130 r5:bf17c000
[ 14.568225] r4:c08af130
[ 14.570778] [<c00097b4>] (do_one_initcall) from [<c0626cc0>] (do_init_module+0x64/0x1b0)
[ 14.578900] r10:bf176e84 r9:edfecd08 r8:1201331c r7:00000001 r6:df5a8080 r5:00000001
[ 14.586799] r4:bf176e84
[ 14.589352] [<c0626c5c>] (do_init_module) from [<c00a3298>] (load_module+0x17cc/0x1e10)
[ 14.597386] r6:edfecd00 r5:00000001 r4:ec52ff48
[ 14.602049] [<c00a1acc>] (load_module) from [<c00a3a7c>] (SyS_finit_module+0x6c/0x7c)
[ 14.609908] r10:00000000 r9:ec52e000 r8:c000fba4 r7:0000017b r6:0002ac84 r5:00000003
[ 14.617806] r4:00000000
[ 14.620357] [<c00a3a10>] (SyS_finit_module) from [<c000fa00>] (ret_fast_syscall+0x0/0x3c)
[ 14.628566] r6:00040000 r5:00000000 r4:00000000
[ 14.633224] Code: ebfffe94 e24bd00c e89da800 e1a0c00d (e92ddff0)
[ 14.639345] ---[ end trace 865ce1654477e3da ]---
/*****************************Segmentation fault also with cmemk***************************/
/etc/rcS.d/S05modutils.sh: line 37: 537 Segmentation fault modprobe cmemk > /dev/null 2>&1
[ 14.930564] cryptodev: driver 1.6 loaded.
[ 15.038205] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
bootlogd: cannot allocate pseudo tty: No such file or directory
Starting random number generator daemon.
[ 15.207686] random: nonblocking pool is initialized
ALSA: Restoring mixer settings...
/usr/sbin/alsactl: load_state:1729: No soundcards found...
hwclock: can't open '/dev/misc/rtc': No such file or directory
Sat Jan 9 06:35:52 UTC 2016
INIT: Entering runlevel: 5misc/rtc': No such file or directory
Starting syslogd/klogd: done
Starting TFT GUI application
Executing the Images still
Export TSLIB Variables
Best Regards,
Ganesh