Tool/software: Linux
Hi,
i want to use the BSL-Scripter on an embedded ARM machine running debian.
How do i build my own scripter on this machine using the source code provided for a linux 32Bit?
On the readme.txt file i found this:
2. Linux
-------------------------------------------------------------------------------
2.1 Development environment
-------------------------------------------------------------------------------
* You will need the GNU tool chain (GCC 4.6.3 or higher) to use the
existing Makefile.
-------------------------------------------------------------------------------
2.2. Dependencies
-------------------------------------------------------------------------------
In order to compile the BSL Scripter with GCC you will need:
* boost
-Download from http://www.boost.org
-Version used in official build is 1.56
-Only libboost_system.a/so and libboost_filesystem.a/so
libboost_program_options-xxx.a/so are required
* hidapi
-Download and build (github.com/.../releases)
-Version used in official build is 0.8.0-rc1
-The BSL Scripter project assumes hidapi being built against libusb-1.0
(the default used in the Makefile coming with hidapi 0.8.0-rc1)
-hidapi.h must be copied to ThirdParty/include/
-hid-libusb.o must be copied to ThirdParty/lib/
So should i copy the source code to my embedded linux and try to build it from there?
How do i build the source code?