Tool/software: Linux
Hello,
I am trying to use the prebuilt images that came with the SDK on a BeagleBoneBlack. The BBB is connected to an HDMI touchscreen. Upon boot the touch screen displays "Please wait...". It never boots the matrix gui though.
I can see that the matrix_browser is listening at port 80. I can even remotely connect to it and it renders in my browser. When I connected to it remotely, it did ask me if a local display was attached, to which I said yes but nothing changed.
It seems to me like the prebuilt image can't find the display. I ran modetest and could see it at connector id 26. So I built the SDK and tried from the built image, same outcome.
I'm pretty sure the HW is OK since the image on the eMMC that came with it runs the display fine.
I'm sure I'm doing something stupid. Any obvious pointers?
Thanks,
Nathan