Tool/software: Linux
Hello, I've been working on a project that uses the processor SDK, and I have made several changes to several u-boot-related files (namely, adjusting the amount/speed of RAM available). These values are inspired by the answer in this post:
e2e.ti.com/.../1926024
I have been invoking the Arago build system with:
MACHINE=am57xx-evm bitbake u-boot --force -c compile
The build will succeed, however the image file will be quite small (680kB or so) and unsurprisingly, refuse to boot. I am unable to receive any kernel messages either.
So, I guess this is more of a general question, but how does one build the processor SDK so it will boot on the EVM?
DETAILS: I am trying to reduce the amount of RAM the AM57x EVM sees by half by only interfacing with one EMIF. I used the sprac36 workbook to alter the EMIF configuration registers, and now I am trying to create a new .img file to boot with.