This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: AM3358 EVM board no device file at /dev/can0

Part Number: AM3358

Tool/software: Linux

Hello

I am currently attempting to enable the DCAN device in the linux kernel,

I have done with the following kernel configuration: 

Networking Support --> CAN bus subsystem support --> Raw CAN protocol <Enable>

  --> Broadcast manager CAN protocol <Enable>

in CAN device drivers -->Platform CAN drivers with netlink support

  --> CAN bit timing calculations <Enable>

--> Bosch D_CAN driver --> Generaic platform bus base d_can Drivers <Enable>

--> CAN devices debugging messages <Enable>

After compilation and downloading uImage to AM3358 EVM board  no device file at /dev/can0. Profile switch is at profile 1

Please let me know if i missed anything.

regards

Shyam