Tool/software: Linux
Hi Community Members,
I am using latest TI-SDK ti-processor-sdk-linux-am335x-evm-03.02.00.05 with a custom AM335x board.
The issue is that the board is not getting powered off with shutdown -h now . Also it is not getting reboot with the init 6. Due to this issue rtcwake is also not working.
INIT: Sending processes the TERM signal
INIT: SendiStopping telnet daemon.
Stopping system message bus: [ 34.477141] ***omap_rtc_alarm_irq_enable***
hwclock: RTC_SET_TIME: Invalid argument
Error opening /dev/fb0: No such file or directory
Stopping syslogd/klogd: no syslogd found; none killed
Stopping thttpd.
ALSA: Storing mixer settings...
/usr/sbin/alsactl: /usr/lib/libasound.so.2: no version information available (required by /usr/sbin/alsactl)
Deconfiguring network interfaces... ifdown: interface lo not configured
ifdown: interface eth0 not configured
done.
[ 35.548679] wlcore: using inverted interrupt logic: 8
[ 35.616986] wlcore: PHY firmware version: Rev 8.2.0.0.224
[ 35.719342] wlcore: firmware booted (Rev 8.9.0.0.31)
[ 35.735367] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
udhcpc (v1.24.1) started
Sending discover...
Sending discover...
Sending discover...