Other Parts Discussed in Thread: AM3352, TPS2051B, TPS2051
Tool/software: Linux
We connect the usb ethernet chip lan9500 to am3352 with newest sdk
there is one board ,it always report such error what is wong ?
[ 13.183492] musb-hdrc musb-hdrc.1.auto: new USB bus registered, assigned bus number 2
[ 13.206436] hub 2-0:1.0: USB hub found
[ 13.210284] hub 2-0:1.0: 1 port detected
Starting Synchronize System and HW clocks...
[[0;32m OK [0m] Reached target System Time Synchronized.
[[0;32m OK [0m] Started Synchronize System and HW clocks.
[ 13.833306] usb 2-1: new high-speed USB device number 2 using musb-hdrc
[[0;32m OK [0m] Reached target System Initialization.
[[0;32m OK [0m] Started Daily Cleanup of Temporary Directories.
[[0;32m OK [0m] Listening on RPCbind Server Activation Socket.
[[0;32m OK [0m] Started DLS test timer.
[[0;32m OK [0m] Reached target Timers.
[[0;32m OK [0m] Listening on D-Bus System Message Bus Socket.
[[0;32m OK [0m] Listening on dropbear.socket.
[[0;32m OK [0m] Reached target Sockets.
[ 14.060873] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_wait_vrise (88, <AValid), retry #3, port1 000a050f
[[0;32m OK [0m] Reached target Basic System.
Starting telnetd.service...
[[0;32m OK [0m] Started Kernel Logging Service.
Starting Permit User Sessions...
[ 14.941082] net eth1: initializing cpsw version 1.12 (0)
[ 14.953029] net eth0: initialized cpsw ale version 1.4
[ 14.975110] net eth0: ALE Table size 1024
[ 14.982559] net eth1: phy found : id is : 0x7c0f1
[ 15.029979] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 15.075665] net eth0: initializing cpsw version 1.12 (0)
[ 15.099128] net eth0: phy found : id is : 0x7c0f1
[ 15.122511] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[[0;32m OK [0m] Started Login Service.
[[0;32m OK [0m] Reached target Network.
[[0;32m OK [0m] Started Omap Server.
Starting Ftp Server...
Starting Network Name Resolution...
[[0;32m OK [0m] Started Getty on tty1.
[[0;32m OK [0m] Started Serial Getty on ttyS0.
[[0;32m OK [0m] Reached target Login Prompts.
Starting rng-tools.service...
[[0;32m OK [0m] Started Ftp Server.
[[0;32m OK [0m] Started Network Name Resolution.
[ 16.417026] random: nonblocking pool is initialized
[[0;32m OK [0m] Started rng-tools.service.
[[0;32m OK [0m] Reached target Multi-User System.
Starting Update UTMP about System Runlevel Changes...
[[0;32m OK [0m] Started Update UTMP about System Runlevel Changes.
DLS login: [ 17.994299] cpsw 4a100000.ethernet eth1: Link is Up - 100Mbps/Full - flow control rx/tx
[ 18.002516] IPv6: ADDRCONF(NETDEV_CHANGE): eth1: link becomes ready
[ 18.114276] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 18.122497] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 18.953540] usb 2-1: device descriptor read/64, error -110
[ 34.183487] usb 2-1: device descriptor read/64, error -110
[ 34.413489] usb 2-1: new high-speed USB device number 3 using musb-hdrc
[ 39.533487] usb 2-1: device descriptor read/64, error -110
[ 54.763489] usb 2-1: device descriptor read/64, error -110
[ 54.993544] usb 2-1: new high-speed USB device number 4 using musb-hdrc
[ 65.413502] usb 2-1: device not accepting address 4, error -110
[ 65.533493] usb 2-1: new high-speed USB device number 5 using musb-hdrc
[ 75.953490] usb 2-1: device not accepting address 5, error -110
[ 75.959654] usb usb2-port1: unable to enumerate USB device
[ 76.183601] usb usb2-port1: over-current condition
[ 76.503492] usb 2-1: new full-speed USB device number 6 using musb-hdrc
[ 78.422025] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 81.783600] usb usb2-port1: over-current condition
[ 82.183494] usb 2-1: new full-speed USB device number 7 using musb-hdrc
[ 85.951800] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_wait_vrise (88, <AValid), retry #3, port1 000b010d
[ 87.463603] usb usb2-port1: over-current condition
[ 87.863493] usb 2-1: new full-speed USB device number 8 using musb-hdrc
[ 90.115936] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 93.143600] usb usb2-port1: over-current condition
[ 93.543561] usb 2-1: new full-speed USB device number 9 using musb-hdrc
[ 95.436875] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 98.823600] usb usb2-port1: over-current condition
[ 99.223544] usb 2-1: new high-speed USB device number 10 using musb-hdrc
[ 101.123722] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 109.763485] usb 2-1: device not accepting address 10, error -110
[ 110.043584] usb usb2-port1: over-current condition
[ 110.443494] usb 2-1: new high-speed USB device number 12 using musb-hdrc
[ 111.776783] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 115.723604] usb usb2-port1: over-current condition
[ 116.123544] usb 2-1: new high-speed USB device number 13 using musb-hdrc
[ 118.058468] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 121.403646] usb usb2-port1: over-current condition
[ 121.683495] usb 2-1: new full-speed USB device number 14 using musb-hdrc
[ 122.023511] usb 2-1: new high-speed USB device number 15 using musb-hdrc
[ 123.848850] musb-hdrc musb-hdrc.1.auto: VBUS_ERROR in a_host (88, <AValid), retry #3, port1 000b010d
[ 127.303619] usb usb2-port1: over-current condition
[ 127.583493] usb 2-1: new full-speed USB device number 16 using musb-hdrc
What does the VBUS_ERROR in a_wait_vrise mean? Is the OTG waiting for the VBus over than 4.6v of the A device threhold?
And what is the state a_host mean?
there is another board ,when we use the old 3.2.0 version it report VBUS_ERROR like the following photo ,are they meet the same error ?