Tool/software: Linux
Hi.
I'm using AM572x custom board
I want to use linux console ttys1 and DSP console use ttys 2.
But, ttys1 & ttys2 are show me linux console same.
then, I want to know how can I remove linux console messages on ttys2 dev.
TTYS1 Log:
U-Boot 2016.05-00118-g68750ff-dirty (Apr 19 2017 - 14:24:54 +0900)
CPU : DRA752-GP ES2.0
Model: TI AM5728 IDK
Board: AM572x IDK REV <NULL>
DRAM: 2 GiB
MMC: no pinctrl for sdr104
no pinctrl for ddr50
no pinctrl for sdr50
no pinctrl for sdr25
no pinctrl for sdr12
OMAP SD/MMC: 0, OMAP SD/MMC: 1
..............................................
intermediate omission
.............................................
***************************************************************
***************************************************************
[ OK ] Started Print notice about GPLv3 packages.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target Network.
Starting Lightning Fast Webserver With Light System Requirements...
cpsw 48484000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
Starting Network Name Resolution...
[ OK ] Started Serial Getty on ttyS1.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Started Network Name Resolution.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Login Service.
[ OK ] Started uim-sysfs.service.
Starting telnetd.service...
Starting tiipclad-daemon.service...
[ OK ] Started telnetd.service.
[ OK ] Started tiipclad-daemon.service.
Starting thttpd.service...
[ OK ] Started thttpd.service.
Starting rng-tools.service...
[ OK ] Started rng-tools.service.
Starting gdbserverproxy.service...
[ OK ] Started gdbserverproxy.service.
Starting thermal-zone-init.service...
[ OK ] Started thermal-zone-init.service.
EXT4-fs (mmcblk0p2): recovery complete
EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am57xx-evm ttyS1
Arago 2016.08 am57xx-evm ttyS1
am57xx-evm login:
TTYS2 LOG:
U-Boot SPL 2016.05-00118-g68750ff-dirty (Apr 19 2017 - 14:24:54)
DRA752-GP ES2.0
Trying to boot from MMC1
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
reading u-boot.img
sootoo23 - Searching Chip.. 'am57xx-beagle-x15'
sootoo23 - Searching Chip.. 'am572x-idk'
Selecting config 'am572x-idk', fdt 'fdt@2'
reading u-boot.img
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am57xx-evm ttyS2
Arago 2016.08 am57xx-evm ttyS2
am57xx-evm login:
Best Regards,
John Kim