Hello. I would like to enable U-Boot to use USB (usbtty) instead of the serial port. I've followed the instructions in U-Boot's README for enabling usbtty; however, I can't get the version of U-Boot supplied with the 137 and 138 to compile when I enable "CONFIG_USB_TTY"
Has anyone been successful in enabling USB console input/output with U-Boot on either the 137 and/or 138? Any help would be appreciated.
Thanks.