Other Parts Discussed in Thread: OMAPL138
Tool/software: Linux
Dear,
My sdk flatform is PROCESSOR-SDK-LINUX-OMAPL138 (4.0.0)
I want to write u-boot & kernel & root-filesystem to nand flash.
At Linux Core U-boot User's Guide, To use nand use commands of 'mtdparts', 'nand erase.part', 'nand write'.
But, 'U-boot' of omapl138 have a problem of MTD.
'mtdparts' command make blow messages (have none mtd information).
For reference, mtd on Linux looks fine like blow.
How to use nand for u-boot & kernel in omapl138-lcdk?
How to add nand mtd partition to u-boot of omapl138-lcdk?
thanks.
Addittion
--------------------------- blow (u-boot) : problem ---------------------------
=> mtdparts
mtdids not defined, no default present
--------------------------------- blow (linux) : OK ------------------------------
root@omapl138-lcdk:~# cat /proc/mtd
dev: size erasesize name
mtd0: 00020000 00020000 "u-boot env"
mtd1: 00080000 00020000 "u-boot"
mtd2: 1ff60000 00020000 "free space"