Tool/software: Linux
Hi all,
I'm trying to recompile the file system following the instructions at processors.wiki.ti.com/.../Processor_SDK_Building_The_SDK.
I use the command "MACHINE=am335x-evm ARAGO_RT_ENABLE=1 bitbake tisdk-rootfs-image" to build, but the process stop with an error.
I've searched through the forum and many times is suggested to copy download and copy the file locally, but I cannot find the file "binutils-native-linaro-2.27-r2016.10".
Searching on internet, I can find binutils-native-linaro-2.27-r2016.08 and looking at the release notes of ti processor SDK 04.00.00 I can see that the Linaro toolchain is 6.2.1 2016.11.
I'd be grateful if someone could help me.
Roberto
This is the output of the console.
Loading cache: 100% |########################################################################################################################################################################| Time: 0:00:09
Loaded 3236 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-16.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "am335x-evm"
DISTRO = "arago"
DISTRO_VERSION = "2017.05"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:3d2f620a6a98b1b6abb1103d7dc986921436ed19"
meta-arago-distro
meta-arago-extras = "HEAD:b727bf8fce8e9cb5a6b5d5b48c45f0088e67eb53"
meta-browser = "HEAD:880a7bd1d3b9a1b2003f5b0620350f03158bbd43"
meta-qt5 = "HEAD:3601fd2c5306ac6d5d0d536e0be8cbb90da9b4c1"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-ti = "HEAD:41d6fdc0fe5ea6054616cfccda13baac3ff33791"
meta-linaro-toolchain
meta-optee = "HEAD:d84874bad834657dd04ea69c35a74dd9dbd535b8"
meta = "HEAD:ddf907ca95a19f54785079b4396935273b3747f6"
Initialising tasks: 100% |###################################################################################################################################################################| Time: 0:00:52
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: binutils-native-linaro-2.27-r2016.10 do_fetch: Failed to fetch URL git://git.linaro.org/toolchain/binutils-gdb.git;protocol=https;branch=linaro_binutils-2_27-branch, attempting MIRRORS if available
ERROR: binutils-native-linaro-2.27-r2016.10 do_fetch: Fetcher failure: Fetch command export DBUS_SESSION_BUS_ADDRESS="unix:abstract=/tmp/dbus-dgxPfDXkLQ"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/signal/TI_SDK/sdk_oe/tisdk/sources/oe-core/scripts/native-intercept:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/texinfo-dummy-native:/home/signal/TI_SDK/sdk_oe/tisdk/sources/oe-core/scripts:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin/x86_64-linux:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/sbin:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/usr/bin:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/sbin:/home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/sysroots/x86_64-linux/bin:/home/signal/TI_SDK/sdk_oe/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/signal/TI_SDK/sdk_oe/gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf/bin:/home/signal/TI_SDK/sdk_oe/tisdk/sources/meta-browser/scripts:/home/signal/TI_SDK/sdk_oe/tisdk/sources/oe-core/scripts:/home/signal/TI_SDK/sdk_oe/tisdk/sources/bitbake/bin:/home/signal/TI_SDK/ti-processor-sdk-linux-rt-am335x-evm-04.00.00.04/linux-devkit/sysroots/x86_64-arago-linux/usr/bin:/home/signal/bin:/home/signal/.local/bin:/usr/local/sbin:/usr/local/bin:/usr/sbin:/usr/bin:/sbin:/bin:/usr/games:/usr/local/games:/snap/bin"; export HOME="/home/signal"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git.linaro.org/.../binutils-gdb.git /home/signal/TI_SDK/sdk_oe/tisdk/downloads/git2/git.linaro.org.toolchain.binutils-gdb.git --progress failed with exit code 128, output:
Cloning into bare repository '/home/signal/TI_SDK/sdk_oe/tisdk/downloads/git2/git.linaro.org.toolchain.binutils-gdb.git'...
fatal: unable to access 'git.linaro.org/.../': error setting certificate verify locations:
CAfile: /tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sy
ERROR: binutils-native-linaro-2.27-r2016.10 do_fetch: Fetcher failure for URL: 'git://git.linaro.org/toolchain/binutils-gdb.git;protocol=https;branch=linaro_binutils-2_27-branch'. Unable to fetch URL from any source.
ERROR: binutils-native-linaro-2.27-r2016.10 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/signal/TI_SDK/sdk_oe/tisdk/build/arago-tmp-external-linaro-toolchain/work/x86_64-linux/binutils-native/linaro-2.27-r2016.10/temp/log.do_fetch.2951
ERROR: Task (virtual:native:/home/signal/TI_SDK/sdk_oe/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils_linaro-2.27.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 871 tasks of which 870 didn't need to be rerun and 1 failed.
Summary: 1 task failed:
virtual:native:/home/signal/TI_SDK/sdk_oe/tisdk/sources/meta-linaro/meta-linaro-toolchain/recipes-devtools/binutils/binutils_linaro-2.27.bb:do_fetch
Summary: There was 1 WARNING message shown.
Summary: There were 3 ERROR messages shown, returning a non-zero exit code.