Tool/software: Linux
Hello All
My board is am335x-evm, SDK is sdk-02.00.00.11.
I have one problem.
serial receive data is lost.
When I lose data I checked as follows:
root@am335x-evm:/proc/tty/driver# cat OMAP-SERIAL
serinfo:1.0 driver revision:
0: uart:OMAP UART0 mmio:0x44E09000 irq:158 tx:45439 rx:110 RTS|CTS|DTR|DSR
1: uart:OMAP UART1 mmio:0x48022000 irq:159 tx:174 rx:1560957 pe:2 RTS|CTS|DSR|CD|RI
root@am335x-evm:/proc/tty/driver#
0: uart:OMAP UART0 mmio:0x44E09000 irq:158 tx:45439 rx:110 RTS|CTS|DTR|DSR
1: uart:OMAP UART1 mmio:0x48022000 irq:159 tx:174 rx:1560957 pe:2 RTS|CTS|DSR|CD|RI
root@am335x-evm:/proc/tty/driver#
Parity error has occurred twice => pe : 2
I used omap-serial driver.
host is PC, device is printer.
under general circumstances, there seems to be no problem
When transfer data amount is large and busy signal is generated, data lost occurs and data seems to be corrupted...
In order to frequently cause this problem, the serial data is slowly read from the device equipment,
busy situations often occur.
busy situations often occur.
Is this a hardware problem? serial driver issue? firmware issue?
How can i fix this problem?
thank you.