I am trying to recreate the SD card that comes with the EVM. I followed the directions in the Software Developer's Guide. Everything seemed to work correctly up to the time of actually booting the board with the SD card installed. The first time I tried to boot the SD card the kernel seems to start booting and I get Penguin on the LCD. But, there is message that something on MMC can't be found. After some time the LCD goes all blue and no Penguin icon. Boot process is still hung. Then I power down the board and try to reboot again. This time U-Boot can't find MMC card and I get this error:
U-Boot 2009.11 (Oct 14 2010 - 20:37:11)
I2C: ready
DRAM: 64 MB
MMC: davinci: 0
In: serial
Out: serial
Err: serial
ARM Clock : 300000000 Hz
DDR Clock : 132000000 Hz
Net: Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot: 0
Card did not respond to voltage select!
** Can't read from device 0 **
** Unable to use mmc 0:1 for fatload **
Wrong Image Format for bootm command
ERROR: can't get kernel image!
U-Boot >
Any idea what is going on? This has happened on 2 separate OMAP-L1 EVMs.
Regards.