Dear all,
I am trying to use the linux git kernel 2.6.36 on our DM355 based platform. Everything was Ok until i tried to compile cmemk with this kernel. I installed the latest linux utils release :
- LinuxUtils 2.26.00.01
-LinuxUtils 2.26.01.02
But i am still getting the error when i compile cmemk :
WARNING: "arm926_dma_map_area"
Installing the module causes an error.
The cmemk module has a reference to that assembler function when it calls dmac_map_area. Which is defined in cacheflush.h
#define dmac_map_area __glue(_CACHE,_dma_map_area)
This problem has been described in the kernel mailing list but never solved :
http://davinci-linux-open-source.1494791.n2.nabble.com/GIT-Kernel-and-CMEM-2-25-04-10-td5330175.html
The linuxutils that i am using are described as linux 2.6.36 and linux 2.6.37 releases so it should be possible to find a solution.
Does anyone faced that problem too ?
Thanks
--
Pierre