Hi,
I wanted to access the pins on the expansion header as GPIO on the Beagle Board xM with Angstrom distribution....
I used the program on this link :
http://linuxjunk.blogspot.com/2009/01/beagleboard-gpio-input-driverless.html
It got compiled and an exe is made using Linux DVSDK....
But when I try running it on the Beagle Board xM with Angstrom distribution :
I got the following error :
./gpio: line 1: syntax error: "(" unexpected
Please tell me where I am wrong...
Regards