Hello,
When using multiple serials in the OMAP L-138 EVM, in u-boot, I have confusion as to the following definition in da850evm.h:
70 #define CONFIG_SYS_NS16550_CLK clk_get(DAVINCI_UART2_CLKID)
the same clock will be used for all UART'S so why should it depend on UART2 only (UART2 is the console) ?
Regards,
Ran