• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » Linux » Linux forum » All Tags » 2.6.29
Share
Linux
  • Forum

Browse by Tags

Linux

Welcome to the Linux Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
2.6.29
  • 1080 video encoding DM6467
  • 1080i
  • 1080i encode
  • 1080p
  • 1080p codecsapp
  • 1080P kernel dm6467
  • 115200n8 root=/dev/nfs rw nfsroot=192.168.1.103:/home/realtimedsp/workdir/filesys ip=192.168.1.3:192.168.1.103:192.168.1.1:255.255.255.0::eth0:off eth=00:40:01:2B:64:60 video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16
  • 138 Nand Flash U-Boot
  • 1808 embedded linux ethernet network AM1808
  • 2.6.18 sdhc
  • 2.6.32 kernel
  • 2.6.32 kernel usb dm6446
  • 2.6.37
  • 2.6.37 kernel
  • 2.6.37 kernel am3715evm camera
  • 2.6.37 kernel usb gadget
  • 2.6.37 kernel usb gadget.
  • 3.0.8+ kernel module usb gadge
  • 3.0.8+ kernel module usb gadget.
  • 3.2.0 linux kernel
  • 3530
  • 3730
  • 4.01.00.09
  • DM355
  • i2c
Related Posts
  • Forum Post: Re: Advice on I2C

    Ankit Mutha Ankit Mutha
    hello stefan, Stefan Gachter I have successfully implemented a test program with the i2c-dev framework. I'm looking do the same but its not working, can you explain how were you able to do that exactly. I'm using kernel 2.6.29 and I'm trying to write a userspace program to interface...
    on Jul 5, 2010
  • Forum Post: RE: OMAP-L138 SOM: UART1 access

    francis kumar francis kumar
    Hello michael, I am also facing similar issue on UART1. I am getting data from GPS (UART1 interface) on RX line, But i am not able to send any data on TX line. I have commented below line. __raw_writel(0, IO_ADDRESS(DA8XX_UART1_BASE) + 0x30); Have you rectified this issue. Please help me, how...
    on Jul 20, 2012
  • Forum Post: RE: OMAPL138 to AM1808

    francis kumar francis kumar
    Hi All, I am using AM1808 and booting the Kernel and Application via SD-Card. I am using RTC for time stamp. AM1808 has internal RTC which we have given the CMOS battery for RTC backup. i.e CR2032 battery one. But I am worried about battery back is not coming for 1 year. it is coming for just 4...
    on Oct 6, 2012
  • Forum Post: Kernel gets hang without RTC battery

    francis kumar francis kumar
    Hi All, I am using AM1808 and booting the Kernel and Application via SD-Card. I am using RTC for time stamp. AM1808 has internal RTC which we have given the CMOS battery for RTC backup. i.e CR2032 battery one. But I am worried about battery back is not coming for 1 year. it is coming for just 4...
    on Oct 6, 2012
  • Forum Post: Chips Select goes high in between every word in SPI transfer

    Erik Rosengren Erik Rosengren
    I'm using the McSPI2 master SPI on an OMAP3 board, running Linux kernel v. 2.6.29. My problem during read/write on the SPI is that the CS goes high in between every transfer word (8 bits). Why is this happening and how can I prevent it? Screenshot:
    on Oct 29, 2012
  • Forum Post: Mini USB support in AM1808 with PC

    francis kumar francis kumar
    Hi All, I am using AM1808 which is running the file system over SD-Card. I have configured the Mini USB driver as mass storage as device. When i am connecting this AM1808 device to computer in Linux it shows "Linux File-CD Gadget". But is not accesing the drive. If it is connecting...
    on Sep 21, 2012
  • Forum Post: RE: Camera Interface with AM1808

    francis kumar francis kumar
    Hi, In 'MT9T031' datasheet there is 'Frame Valid', 'Line Valid' and 'Strobe' three signals are going to some where. I am interfacing these signals to my AM1808 Processor. Could you please find out where should i interface these two signals in my AM1808 processor...
    on Nov 29, 2012
  • Forum Post: RE: Fonts installing in AM1808

    francis kumar francis kumar
    Hi All, Please help me how to see local langues in AM1808. Any required font libraries need to cross compile. Thanks, Francis
    on Dec 3, 2012
  • Forum Post: Camera Interface with AM1808

    francis kumar francis kumar
    Dear All, I am working on AM1808 processor. I would like to add ‘ Camera’(3Mega Pixel) features to this processor. Will this processor supports camera feature. If supports please tell me the supported Camera part number and corresponding kernel & test application. Thanks...
    on Nov 29, 2012
  • Forum Post: RE: stability of ext2 file system on SD Card

    francis kumar francis kumar
    Hi, I am also having similar issue I am using AM1808 processor(Linux 2.6.32). It has 1 USB Host + 1 mini USB feature is available. Before mini USB, the main Host USB is working fine in my AM1808 I can see the files in my Pen-drive. When i added mini USB driver, both are working some time, after...
    on Jan 25, 2013
  • Forum Post: RE: UART2

    francis kumar francis kumar
    Hi, I am using AM1808 processor. UART0, UART1 already used in my application. there is only choice UART2 which i need to interface this to our EXTENAL thermal serial printer. I can see all the kernel log in PC console, The same UART2 i want to connect to drive my printer. I will disconnect the...
    on Jan 30, 2013
  • Forum Post: kernel log when boot up?

    nikunj rudani nikunj rudani
    hello there, My system has DM365 working on "MontaVista 4.2.0-16.0.32.0801914" and kernel is "Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le". and i want to see kernel log on terminal (uart com9) from when boot start, so can any one suggest what i need to change in kernel...
    on Mar 14, 2013
  • Forum Post: RE: linux hangs at "Uncompressing Linux... done, booting the kernel." with XAM3359ZCZ custom board

    Sekra Invos Sekra Invos
    Thankyou for your reply.. I get that linux-3.3.7 from the http://www.ti.com/tool/linuxezsdk-sitara for Linux EZ SDK for BeagleBoard-xM . After Linux 2.6.37+ supports the console ttyO2 (capital O) not S.But i tried both the console but doesn't happens in my minicom terminal.I tried all those things...
    on Apr 22, 2013
  • Forum Post: RE: linux hangs at "Uncompressing Linux... done, booting the kernel." with XAM3359ZCZ custom board

    Sekra Invos Sekra Invos
    Hello Renjith I tried both the uboot,kernel-3.37 from the same package but shows the same result and hangs up.As per u told i disable some of the drivers (USB,capture) it gives 2.7MB of kernel size. From the driver: i enable earlyprintk option also. My bootargs environment is - OMAP3 beagleboard...
    on Apr 22, 2013
  • Forum Post: RE: Linux kernel build for DM36x fails...

    Sekra Invos Sekra Invos
    Hello phillip,prabhakar and Ravi I'm sekra...im working in Linux kernel 3.3.7...I am stucked out in this problem few days back.if you are in this same problem..this may be helpful to you... Your Toolchain is right but version may be collapse or overwhelm your codes because OMAP,davinci media...
    on Apr 23, 2013
  • Forum Post: RE: Camera drivers

    Sekra Invos Sekra Invos
    Hai I'm using Linux kernel 3.2.xx stable kernel.Now i'm working on Camera driver.Now i add one driver for the camera i'm using.It s based on I2C protocol.So in that Kconfig i wrote as depends on I2C && VIDEO_V4L2 , But during compilation it shows a serious error.Modules doesn;t...
    on May 7, 2013
  • Forum Post: Camera drivers

    Sekra Invos Sekra Invos
    Hai I'm Sekra I am using one davinci processor which was running on linux kernel.I had a serious doubt with the kernel drivers In "Multimedia support" options.......... there is a for camera drivers....Lot of the types were there..... what is the difference between CAMERA SENSOR...
    on May 6, 2013
  • Forum Post: Beagleboard xm camera support

    Sekra Invos Sekra Invos
    Hai I'm Sekra I'm using Omnivision 2 megapixel camera (SOC camera supported CMOS sensor) ans im using 3.2.44 mainline kernel. I want to write the drivers for the camera working on my beagleboard xm board. In kernel, the V4L2 camera support for CONFIG_VIDEO_XXX and CONFIG_SOC_CAMERA_SUPPORT...
    on May 14, 2013
  • Forum Post: Linux kernel compilation for camera

    Sekra Invos Sekra Invos
    Hai When i compile the board-omap3beagle-camera.c,i get the following errors in mux file. arch/arm/mach-omap2/mux.h:96: error: redefinition of 'struct omap_board_data' arch/arm/mach-omap2/mux.h:113: error: redefinition of 'struct omap_mux_partition' arch/arm/mach-omap2/mux.h:131:...
    on May 17, 2013
  • Forum Post: Kernel takes time to BOOT

    Sekra Invos Sekra Invos
    Hai I'm Sekra When i compile any kernel from kernel.org source website. When i make any uImage from any of those kernels.When i boots up the linux the uboot loads immediately. Entry Point: 80008000 Verifying Checksum ... OK OK Starting kernel ...... After the above indication in my console...
    on May 21, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use