• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » Linux » Linux forum » All Tags » DM3730
Share
Linux
  • Forum

Browse by Tags

Linux

Welcome to the Linux Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
DM3730
  • am1808
  • am3517
  • arago
  • ARM
  • audio
  • boot
  • codec engine
  • DaVinci
  • daVinci dm365
  • DM355
  • DM365
  • DM365 + DVSDK
  • DM368
  • dm6467
  • driver
  • dsplink
  • DVSDK
  • GPIO
  • GStreamer
  • Kernel
  • Linux
  • Linux driver
  • Linux Drivers
  • Linux Kernel
  • NAND
Related Posts
  • Forum Post: MP4V-ES running on DM3730 EVM- (TMDXEVM3730) - CPU resource issue seen when encoding --

    Rick Bogdan Rick Bogdan
    DWe are currently running a Telephony application on the DM3730 ( TMDXEVM3730) eval board. The video quality is ok on the receiving end except for some video glitches here and there. However, a bigger problem exists on the Video encoding side. We seem to be running out of cpu or the cpu is not...
    on Dec 10, 2010
  • Forum Post: Re: SmartReflex on DM3730EVM

    Kanae Kanae
    Dear Sanjeev, Thank you for your reply. Here is the information from the board. <Silicon revision> CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f <cpuinfo> root@dm3730-am3715-evm :~# cat /proc/cpuinfo Processor : ARMv7 Processor rev 2 (v7l) BogoMIPS : 998.84 Features...
    on Feb 16, 2011
  • Forum Post: Re: SmartReflex on DM3730EVM

    Kanae Kanae
    Dear Sanjeev, Thank you for pointing that out. Silicon revision is "OMAP3630/DM3730 ES1.0 (l2cache iva sgx neon isp 192mhz_clk )". This is same as your example. Reagards, Kanae
    on Feb 17, 2011
  • Forum Post: [dm37x-evm] how to use locale?

    KANG JIN HO KANG JIN HO
    Hello, I'm setup the Linux dm37x-evm use dvsdk_dm3730-evm_4_01_00_09_setuplinux file. I want use locale & localedef, but not found now. Can I anyone? Thanks. ======================================================================= root@dm37x-evm:/ # uname -a Linux dm37x-evm 2...
    on Feb 18, 2011
  • Forum Post: Working with 256MB SDRAM and Codec Engine

    Glenn Wainwright Glenn Wainwright
    I'm on a DM3730 board with 256MB SDRAM instead of the normal 128MB. Following the guides, my bootargs are set up as: setenv bootargs mem=99M@0x80000000 mem=128M@0x88000000 console=ttyS0,115200n8 noinitrd rw ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}:eth0:on root=/dev/nfs nfsroot...
    on Mar 22, 2011
  • Forum Post: DVSDK 4.01 on IGEPv2 RC4

    Jordi Frances Jordi Frances
    Hi, I am interested in running DVSDK 4.01 on IGEPv2 RC4 (based on DM3730). An out-of-the box compilation does not boot (uboot gets stuck at "kernel loaded" when the kernel is supposed to take control). I tried to build DVSDK around another kernel ( 2.6.35.11 provided by IGEPv2 manufacturer...
    on Mar 21, 2011
  • Forum Post: Re: how to create dsp server?

    Siddharth Heroor Siddharth Heroor
    Hi, yin yu I use the DM3730 board,but now I need the dsp server ,and how I can make the dsp server to run on the arm core? thanks! I'm assuming you need more information on Codec Engine and how to interface to the DSP. Please refer the Codec Engine documentation in the codec engine directory...
    on May 12, 2011
  • Forum Post: Re: ULPI-PHY initialisation and to read-write data packets

    Anup Kumar Anup Kumar
    Ajay, Thanks for the drivers. I have a more specific question.Using DM3730 We want to communicate to USB 3320(transceiver) which is present on the same board (Beagle board-xM). which mode should we use- ULPI_PHY mode or the ULPI_TLL mode? regards.
    on Jun 24, 2011
  • Forum Post: Re: ULPI-PHY initialisation and to read-write data packets

    Anup Kumar Anup Kumar
    To send data/commands to a PHY (USB3320) from DM 3730(on Beagleboard) is it possible only through sending Packets? If so how to generate packets? kindly help. regards, Anup.
    on Jun 27, 2011
  • Forum Post: Re: DM37X eval module kernel panics

    rere rere
    Hi, we join the discussion, 'cause we found a similar scenario. kernel: 2.6.32 - PREEMPT (PSP 03.00.01.06) customized for our new platform DM3730-clone filesystem: Arago 2009.11 Thanks in advance Christian Ambrogio ------------------------------------------------------ --...
    on Jul 12, 2011
  • Forum Post: Re: Power managemnet: core and per do not hit OFF/Retention state

    DaveB123 DaveB123
    Are you using a custom board or an EVM? I am assuming you mean DM3730. TI has split the OMAP naming to AM37xx and DM37xx. If you are using an Mistral EVM, make sure it is Rev G or higher and has the most recent silicon module (Hynix memory Silicon rev 1.1)
    on Jul 14, 2011
  • Forum Post: Re: spidev_test in l138

    Pradeep TR Pradeep TR
    hi, hope the way to use it is #./spidev_test -D /dev/spidev1.0 -l ,this "-l" was missing I beleive ,but for me even after giving it am getting just "ff ff " am making use of the same bus number and chip select to which we have connected the spi falsh, and have set the EVM boadr...
    on Jul 25, 2011
  • Forum Post: Suspend/Resume beagleboard-xm revC Sitara SDK 05.02.00.00

    Jeffrey Beaupre Jeffrey Beaupre
    Hi, I recently installed the prebuilt images for the beagleboard that came with the 5.02 EZ SDK. It seems the suspend to memory does not work "out of the box" in these images. After echo mem > /sys/power/state the system suspends its disk, and the hangs. If i hit ctrl-c it continues...
    on Jul 28, 2011
  • Forum Post: How to configure TVP5150 driver for the NTSC input

    Pratik Shinde Pratik Shinde
    Dear All, I have a DM3730 board (IGEPv2). I am trying to take analog video input through TVP5151, the module is tvp5150.Currently its working for the PAL standards. The original driver tvp5150 - Texas Instruments TVP5150A/AM1 video decoder driver by Mauro Carvalho Chehab (mchehab@infradead.org...
    on Aug 10, 2011
  • Forum Post: Re: DM365 DMAI Osd capabilities

    Danfeng Lu Danfeng Lu
    on Aug 17, 2011
  • Forum Post: Activating camera input on the DM37x eval board

    Paul Chiha Paul Chiha
    I don't know how to select my on board LI module camera as input (instead of the default TVP5146). I've seen in the documentation that GPIO 157 needs to be low. And I've also been able to force this line low via /sys/class/gpio/gpio157. However, VIDIOC_ENUMINPUT always comes back with...
    on Aug 22, 2011
  • Forum Post: TPS65930 USB Driver Problem~

    yuliang yuliang
    Hi Guys; We have a new board of DM3730 ,and the OTG use TPS65930 's USB ports.On DM3730 EVM board,it's use ISP1507.Now we use the DM3730 EVM BSP software to our new board.When compile the kernel ,i add the TWL4030 USB driver .After boot the system ,plug a USB storage in OTG port on our board...
    on Aug 30, 2011
  • Forum Post: Re: To change EVM code of TI814X-LINUX-PSP-04.01.00.05 to support the RMII mode on custom board

    Pradeep TR Pradeep TR
    Hi, Using the EVM TI8148 which has phy in MII mode, now we have moved to our custom board. After Kernel comes up want to configure Phy in MII mode because the hardware has support only for it. How to go about it ? Is it enough if the below code is added So now to make our custom board work...
    on Sep 26, 2011
  • Forum Post: Re: PSP4.02.00.07: System freezes on watchdog timer triggers

    R1234 R1234
    I'm facing this issue too? Any solutions?
    on Oct 14, 2011
  • Forum Post: DM3730 ISP entity problem

    lionel hsiao lionel hsiao
    I use PSP04.02.00.07. After linux kernel 2.6.37 start. I can see ISP driver and mt9p031 finished. In the console. I run #ls /dev/video* /dev/video0 /dev/video2 /dev/video4 /dev/video6 /dev/video8 /dev/video1 /dev/video3 /dev/video5 /dev/video7 #media-ctl -p Opening media device /dev...
    on Oct 18, 2011
  • Forum Post: Re: DM3730 X-Loader code via UART3 (Serial Boot).

    Michael T Michael T
    The Flash Tool that is available here supports NAND programming via UART3 or USB. http://www.ti.com/tool/flashtool Regards, Michael T
    on Oct 31, 2011
  • Forum Post: ti-sdk-am37x-evm-05.02.00.00 on CCSv5

    Bigtree Bigtree
    Hi Experts, I am using Code Composer V5 (CCSv5) and Linux tool chain ti-sdk-am37x-evm-05.02 and I am new to this. I was trying to setup interrupt using interrupt.h in Linux kernel. But I found /linux/interrupt.h is missing from the /user/include/linux directory in Code Composer. By further debugging...
    on Oct 26, 2011
  • Forum Post: Waiting for service media.audio_policy... Issue

    lionel hsiao lionel hsiao
    I download AM35x-OMAP35x-LINUX-PSP-04.02.00.07 and almost time I got "Waiting for service media.audio_policy..." forever loop. Sometimes it continue to work. your comment? ************************************************************************** -------- beginning of ...
    on Nov 11, 2011
  • Forum Post: DVI Display Issue on DM3730 EVM

    Jeffrey Vertosick Jeffrey Vertosick
    I am using DVSDK 4.02 with a DM3730 EVM. I am attempting to use the DVI output to pass 24-bit data from the DM3730 to an external FPGA. The data I am passing consists of 16-bits of YUV data + 8-bits of additional data. So I am copying the Y values into the R bytes of frame buffer fb0, the U/V data into...
    on Nov 18, 2011
  • Forum Post: U-boot hangs while reading DM3730 DSS registers locations

    anik anik
    Hi All, I am trying to read the DSS registers using "md" command of u-boot, it is hanging there. I am working on DM3730 processor. Exapmple:- ----------------------------------------------------- OMAP3EVM # md 0x48050400 0x1 48050400: ----------------------------------...
    on Nov 25, 2011
123
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use