• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Embedded Software » Linux » Linux forum » All Tags » arago
Share
Linux
  • Forum

Browse by Tags

Linux

Welcome to the Linux Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
arago
  • am1808
  • am3517
  • ARM
  • boot
  • DaVinci
  • daVinci dm365
  • DM355
  • DM365
  • DM365 + DVSDK
  • DM368
  • dm6467
  • driver
  • DVSDK
  • GPIO
  • GStreamer
  • Kernel
  • Linux
  • Linux driver
  • Linux Drivers
  • Linux Kernel
  • NAND
  • OMAP L137
  • OMAP L-137
  • OMAP L138
  • OMAP_L138
Related Posts
  • Forum Post: Building Arago file system

    Constantine Constantine
    I tried to build file system with Arago project accordingly http://wiki.davincidsp.com/index.php/DaVinci_PSP_03.01_Phase_2_Release_Notes . I installed required packages on my Ubuntu 9.10 with sudo apt-get install help2man diffstat texi2html texinfo In addition to sample environment configuration...
    on Nov 23, 2009
  • Forum Post: Two questions : I2c error and arago install.

    yonghui chen yonghui chen
    when I use NFS to boot dm365 and run the encode demo. It prints follow message. root@192.168.0.222:/opt/dvsdk # ./encode -v test.264 -y 2 Encode demo started. i2c_adapter i2c-0: tvp514x_setinput:lost lock] i2c_adapter i2c-0: tvp514x_setinput:lost lock] i2c_adapter i2c-0: tvp514x: no input connected...
    on May 18, 2010
  • Forum Post: dm365: arago kernel image boot issue

    Arun12185 Arun12185
    Hello, I downloaded the latest arago-davinci kernel source, reconfigured (no code changes done) and programmed the uImage. What is happening is the image gets transferred to the board over TFTP successfully and after the u-boot message 'starting kernel' the boot process starts all over...
    on Jun 10, 2010
  • Forum Post: arago / DM365

    WingEdLizard WingEdLizard
    I've been trying to build php on arago, and I keep getting problems: | Building with SSL | ln -s ssl_unix.c osdepssl.c | echo -I/home/brettb/oe/arago-tmp/sysroots/armv5te-none-linux-gnueabi/usr/include/openssl -I/home/brettb/oe/arago-tmp/sysroots/armv5te-none-linux-gnueabi/usr/include/openssl...
    on Jun 28, 2010
  • Forum Post: TSC2007 No IRQF_TRIGGER set_type function for IRQ 44 (AINTC) DM365

    Ali Bingöl Ali Bingöl
    Hi I have problems with TSC2007 on DM365. DM365 recognized TSC2007 device via I2C at address 0x0a. But the problem is i couldn't set GPIO0 as an IRQ 44. the code is below. I am working with linux-2.6.18_pro MVL kernel. And the driver is an example driver which i downloaded from tsc2007 download...
    on Jul 19, 2010
  • Forum Post: DM365 TSC2007 problem

    Ali Bingöl Ali Bingöl
    hi I have problem on TSC2007 driver on DM365. I Couldn't introduce TSC2007 to DM365. I get nothing when i type "cat /proc/bus/input/devices" and tslib gives same error "no such device". I looked to pins of TSC2007, PENIRQ, SDA and SCL are being seen as it should be via scope...
    on Jul 9, 2010
  • Forum Post: serial flash,sfh_DM36x, for oneNAND flash

    Rami Nissim39095 Rami Nissim39095
    I am using the DM365 with DVSDK3.10 & have to work with oneNAND on DM365 EVM. I got an error during the serial_flash procedure. (sfh_DM36x.exe, - see below): Waiting for SFT on the DM36x... Target: Starting UART Boot... Target: BOOTUBL BOOTUBL commmand received. Returning CMD and command... CMD...
    on Jul 6, 2010
  • Forum Post: Re: Building ARAGO

    Michael Erickson Michael Erickson
    I too am seeing this issue. I am also using CodeSourcery G++ lite (arm-2010.09). I am tracking the stable branch of arago, arago-bitbake, and arago-oe-dev.
    on Dec 28, 2010
  • Forum Post: udev rules for USB memory stick

    KB2603 KB2603
    Hi, I am using dvsdk4.0 for DM365 processor. I am trying to set a rule within udev that will launch a shell script when a USB memory stick is connected. With root privilege, I have placed in /etc/udev/rules.d/ folder the rule script with a name: 99-usbdetect.rules. 99-usbdetect.rules file is...
    on Mar 8, 2011
  • Forum Post: Re: JFFS2 file system query for OMAPL137

    Jitendra Jagasia Jitendra Jagasia
    Hi Gururaja, Thanks for you reply. I had tried the above given procedure but it gives me the following errors jffs2_scan_eraseblock () : Magic bitmask 0x1985 not found at 0x0037c024: 0x6373 instead JFFS2 warning: (1) jffs2_do_read_inode_internal : Truncating ino #392 to 23300 bytes failed...
    on Mar 28, 2011
  • Forum Post: Total Ram size is less than total Ram allocated to EVM OMAPL137

    Jitendra Jagasia Jitendra Jagasia
    Hi, I have a query regarding the total amount of ram available to EVM OMAPL137 during runtime of Linux but according to the Uboot command " bootargs mem=32M " I have allocated 32MB of ram to the EVM OMAPL137 but during runtime when I run " free " command on Linux it displays...
    on Apr 6, 2011
  • Forum Post: Arago repositories

    Marlon Smith Marlon Smith
    Hi everyone, I'm running the Arago build that comes with the latest dvsdk. The platform I'm using is the DM365 development kit. I'm using the Qt demo browser, and would like to install the totem-browser-plugin. This package is listed in the Angstrom repositories, and it is my understanding...
    on Apr 7, 2011
  • Forum Post: Re: LCD Splash Support in U-Boot (AM3517)

    David Paden David Paden
    Well, it looks like I'll be working on this in the near future. I'll look in to the link you sent me as soon as I can. How similar is the Beagle's DSS system to the AM3517? Is the register layout the same?
    on May 10, 2011
  • Forum Post: Re: Need TFT LCD Driver support

    francis kumar francis kumar
    Hi, I made a changes in LCD configuration and LCD panel timing parameter. But i am not sure with these changes driver will work or not. What i am using the LCD Panel doesn't have VSYNC and HSYNC supported signals. It is having DE(data enable signal) and clock. Remaining the same pin configuration...
    on May 17, 2011
  • Forum Post: Error in enabling SPI1 of OMAPL137 EVM board

    Jitendra Jagasia Jitendra Jagasia
    HI, I am using EVM OMAPL137 board & Linux. EVM OMAPL137 has two SPI peripheral. SPI0 of EVM board is used for SPI0 Flash & in the kernel for OMAPL137 only SPI0 is defined But in our application we require SPI1 also. So in kernel files I have made some changes as given below ...
    on May 18, 2011
  • Forum Post: Re: Building arago with small rootfs size

    Siddharth Heroor Siddharth Heroor
    Hi, There are a couple of options. 1. From Arago you can also build images that are present in OE. So, an image that you find to be useful in arago-oe-dev/recipes/images can be built via bitbake as well. 2. Once you build an image, you can query the opkg database and use opkg to remove software...
    on Jun 3, 2011
  • Forum Post: Re: spidev_test in l138

    Pradeep TR Pradeep TR
    hi, hope the way to use it is #./spidev_test -D /dev/spidev1.0 -l ,this "-l" was missing I beleive ,but for me even after giving it am getting just "ff ff " am making use of the same bus number and chip select to which we have connected the spi falsh, and have set the EVM boadr...
    on Jul 25, 2011
  • Forum Post: Unable to load PRU firmware for EVM OMAPL137 with new ramdisk.

    Jitendra Jagasia Jitendra Jagasia
    Hi, I am currently working on EVM OMAPL137 & Linux kernel is used in the system. EVM OMAPL137 have PRU system. I have a serial daughter card for EVM OMAPL137 & I have tested the PRU serial expansion card by applying patch to the Linux kernel & loading the PRU module. The PRU system...
    on Jul 12, 2011
  • Forum Post: LCD Splash Support in U-Boot (AM3517)

    David Paden David Paden
    Hello, I need to get a splash screen displayed on our LCD ASAP after power on. Currently, there appears to be NO display support in U-Boot for the OMAPs. I was looking at the omapfb support in the Linux kernel and it looks very complicated to others I've worked with in the past. Is there any...
    on May 6, 2011
  • Forum Post: OpenGL ES 1.1/2.0 (3D Graphics) will support AM1808 processor

    francis kumar francis kumar
    Hi, I just want to know whether AM1808 will support “ OpenGL ES 1.1/2.0 (3D Graphics) ” feature for Qt Graphics application. Please provide me Qt configuration settings using with this feature. Regards, Francis Kumar.B
    on Sep 7, 2011
  • Forum Post: Re: To change EVM code of TI814X-LINUX-PSP-04.01.00.05 to support the RMII mode on custom board

    Pradeep TR Pradeep TR
    Hi, Using the EVM TI8148 which has phy in MII mode, now we have moved to our custom board. After Kernel comes up want to configure Phy in MII mode because the hardware has support only for it. How to go about it ? Is it enough if the below code is added So now to make our custom board work...
    on Sep 26, 2011
  • Forum Post: ti-sdk-am37x-evm-05.02.00.00 on CCSv5

    Bigtree Bigtree
    Hi Experts, I am using Code Composer V5 (CCSv5) and Linux tool chain ti-sdk-am37x-evm-05.02 and I am new to this. I was trying to setup interrupt using interrupt.h in Linux kernel. But I found /linux/interrupt.h is missing from the /user/include/linux directory in Code Composer. By further debugging...
    on Oct 26, 2011
  • Forum Post: How to make sd card for Arago Demo Images for Beagleboard - xM

    Anand Satpute Anand Satpute
    I have a BeagleBoard-xM. I have Downloade the Arago demo files. How should i make the SD card and boot from it? Thanks, Anand.
    on Oct 24, 2011
  • Forum Post: Problem with arago filesystem for PSP 4.02.007 (Beagleboard)

    Anand Satpute Anand Satpute
    I have built the kernel 2.6.37 using PSP 4.02.007 for beagleboard xM. PSP does not include the file system so i tried the demo images of file system from the arago repository. With these images the kernel is not booting. I think this is beacause the demo filesystem images are buid for kernel version...
    on Nov 2, 2011
  • Forum Post: Re: Accessing spidev node on AM1808

    jitendra panchal jitendra panchal
    Hi Matt, I followed the procedure from link you mentioned with the stock kernel & file system but i dint see any spi related node in /dev. Do I need to make any additions in /home/jitendra/ti-sdk-am180x-evm-4.0.1.0/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/mach-davinci/board-da850-evm...
    on Dec 16, 2011
123
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use