I'm asking this because the software manage section of the TI is confusing. I download what is claimed to be the lastest sdk for the DM368 (04_03_00_06), but it says it's for the DM3730 when you install it. The when I go to get the codecs the directory name is for an OMAP processor.
So what's the deal? I just want to make sure I have the latest because I'm getting segmentation faults using H264 encode and there is a thread claiming it's fixed in the newest codecs.
JohnA
Hi John,
The latest DM36x codecs are available on http://software-dl.ti.com/dsps/dsps_public_sw/codecs/DM36x/index_FDS.html
I will check on the SDK confusion point which you mentioned.
regards
Yashwant
Latest H264 Encoder Vesrion : 02.30.00.03
Latest H264 Decoder Version : 02.00.00.13.
There is a possibility that dvsdk may have little older version, you can check following page for latest codecs
http://software-dl.ti.com/dsps/dsps_public_sw/codecs/DM36x/index_FDS.html
And regarding codecs in dvsdk 04.03.00.06 version, we will check with dvsdk team and let you know.
Thanks,
Veeranna
John,
I am not sure if you are following the download links correctly.
The release 04.03.00.06 (New release, released on Dec-11) does not support DM368, The below download link clearly says supported platforms for DVSDK 04.03.00.06
http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_4_00/latest/index_FDS.html
Moreover the installer name must reflect (dvsdk_dm3730-evm_04_03_00_06_setuplinux) platform it is targeted for.
The latest release for DM368 still remain 04.02.00.06, the same can be downloaded via above link by clicking link "DVSDK 4_02" at section "The previous DVSDK 4.xx release(s) can be found: " of the above page.
Please let us know where exactly it misleads, we will correct it.
Thanks & Regards
Velan
Don't forget to verify answers to your forum questions by using the green "verify Answer" button.
Did you read the DVSDK4.x FAQ? If not, PLEASE read it.
VelanJohn, I am not sure if you are following the download links correctly. The release 04.03.00.06 (New release, released on Dec-11) does not support DM368, The below download link clearly says supported platforms for DVSDK 04.03.00.06
Could you please send the link you are using. I am working to categorize this, will try to fix if possible.
Thanks & Regards,
There still is the same problem till today.
The page is http://www.ti.com/tool/linuxdvsdk-dm36x .
Pressing "Get Software" takes you to the: