Hello everyone,I am trying to fix the size of encoding video data by setting it in CBR.But the video data have grown big/small than the value that I set.(setting): 150kbps ---> (real): 560kbps/50kbps
Input sources are snowy noise/black 0%.framerate: 1bitrate: 150kbpsrcAlgorithm: CBRI tried with DM8168DVRRDK. RDK version is 01_09_00_16.Does CBR mean CVBR?How do I fix the size of encoding video data?Would you give any advice?Best RegardsYoji
Yoji,
Can you specify the full encoder parameters, can you also send the i/p and o/p file. Looks like your test sequence comprise of Noise and black data.
regards
Yashwant
Hi Yashwant,
Thank you for a reply.I understood it.I try it.Best regards.
Hi Yashwant,
I changed parameters.The parameters are as follows.
//#define ENC_LINK_DEFAULT_ALGPARAMS_RATECONTROLPRESET (IVIDEO_STORAGE)
#define ENC_LINK_DEFAULT_ALGPARAMS_RATECONTROLPRESET (IVIDEO_USER_DEFINED) // for change rcAlgo
//#define ENC_LINK_DEFAULT_ALGPARAMS_TARGETBITRATE (2 * 1000 * 1000)
#define ENC_LINK_DEFAULT_ALGPARAMS_TARGETBITRATE (200 * 1000) // 200kbps
//#define ENC_LINK_DEFAULT_ALGPARAMS_MAXBITRATE (-1)
#define ENC_LINK_DEFAULT_ALGPARAMS_MAXBITRATE (200 * 1000) // 200kbps but ignored
//params->rateControlParams.rateControlParamsPreset = IH264_RATECONTROL_PARAMS_DEFAULT;
params->rateControlParams.rateControlParamsPreset = IH264_RATECONTROL_PARAMS_USERDEFINED;
params->rateControlParams.rcAlgo = IH264_RATECONTROL_DEFAULT;
params->rateControlParams.rcAlgo = IH264_RATECONTROL_PRC_LOW_DELAY;
But it worked only as VBR.
I'll try more.
Best Regards.
YOJI YASUDA params->rateControlParams.rcAlgo = IH264_RATECONTROL_DEFAULT; params->rateControlParams.rcAlgo = IH264_RATECONTROL_PRC_LOW_DELAY;
Not sure about 'IH264_RATECONTROL_DEFAULT' and 'IH264_RATECONTROL_PRC_LOW_DELAY' values . To enable CBR rate control you need to set params->rateControlParams.rcAlgo = 0.
Please note that if you want enable Perceptual RC you need set it in dynamic param. And it is valid only for encQuality 0 and 1.
Thanks,
Veeranna
Hi Veeranna,
Thank you for a reply.
It is not yet solved.
I set
params->rateControlParams.rcAlgo = 0.
But it works as VBR.
I think
VENC_RATE_CTRL_VBR=0,
VENC_RATE_CTRL_CBR=1.
It was written in "ti_venc.h".
I'll try more in detail.
Best RegardsYoji