Two processes accessing DCE on DRA7xx

Hi,

I have a requirement where two processes needs to be created(each runs on encoding use case). Could you please provide me the following information

1. Is DCE multiinstantiable (can dce_init be done multiple times)

2. If not can I call dce_init() in one process and use the same handle in another process to create the encoding instances

3. If (2) is possible how thread/process safe it is to concurrently access the dce from two different processes?

Thank you inadvance

Regards,

Mahi

3 Replies