We are using H.264 Baseline Profile Decoder 2.00 on a DM6446 (C64x+). This decoder has error concealment supported. The error concealment that is applied does not look good. The desired functionality would be that when a frame has an error it is simply discarded and the previous reference frame is used as the current frame or the MBs that could not be decoded are simply copied from the previous reference frame. I was wondering if there is any way to turn it off? Is there a version that error concealment is not supported?
Jeremy