I'm trying to execute the deinterlacer codec test app i2p_test (from DM3730 DVSDK) on the DM6467. With some project modifications, I have successfully built the app with CCS 4.2.4. When I execute the app it never returns from the call to the codec (handle->fxns->process() which is in the function I2P_frameapply(), in file i2p.c). The codec does not come with source code, so I cannot step into it.
I noticed that the link.i2p.cmd has the following memory definition. I'm not sure if these are correct for DM6467.
L1DSRAM : origin = 0x10f04000, len = 0x10000
DDR2 : origin = 0x80000000, len = 0x01000000
I am using the gel file, davindihd1080p_dsp.gel, from Spectrum Digital. I noticed that this gel file turns off L2 and EDMA, but I'm not sure what settings to use to set those up. Also, I have to connect to the ARM before I connect to the DSP, so I don't know if the ARM gel creates a conflict.
Any help is appreciated.