Hello,
I am using the H264 HP Encoder to encode 1080p and 720p videos. I am using the example videos (airshow) that come with MCSDK_VIDEO. I have duplicated the original videos in order to have 30 frames worth of input instead of 5. I am using settings from the codecParams.cfg file located in the examples/transcode/testVecs/config folder in MCSDK_VIDEO.
When I encode the 1080p version, everything looks ok. When I encode the 720p version using the same settings, the output has blue and green artifacts that appear to be ghost images of the original image. I have attached a video of the output showing the problem I am seeing along with the configuration parameters that I am using. I have also added a screen shot of the issue to the end of this post.
What could be causing these artifacts and why would they show up in 720p but not in 1080p?
Chris
Signalogic