Hi
Firstly, I'd like to confirm how the coh_ratio_threshold parameter is used in practice. According to the API documentation, when the ratio is exceeded for a number of frames a 'coherence presence' is detected. The AER developer guide does not seem to describe these parameters and events in any more detail.
What does a 'coherence presence' detection signify? Is this related to the coherence of the acoustic system (the echo path) being considered suitably linear and free of noise to allow convergence of the adaptive filter? Or is it related to something else, e.g. LMS misalignment?
In short, do we want to maximise the number of coherence events or minimise them?
Secondly, can you describe further to the API description how the clip_scale_curve is applied? Is the input to the curve the double talk detection value? Presumably the input value compared against the 4 thresholds, but what is then scaled by 4,1,1 or 0 depending on which range the input falls within (c1-c4)?
Kind regards,
Simon