Hello,
I am using the C674x AAC-LC Encoder XDAIS Module (V01.00.01 ELF) in an OMX-Environment (DM8168), which is running stable in single-channel-mode (mono). When configuring as stereo, the module crashes after some hours of continuous encoding (2ch, 48000kHz, 4096 byte/period). Currently I am trying to isolate the error, but what I know is that the error occurs in the OMX Code on the DSP, which mainly calls AUDENC1_process().
My Questions:
- Are there any issues/limitations/bugs known for stereo-AAC-LC.
- Is there a newer version than V01.00.01 (ELF) of this module around?
Thanks,
Wolfgang