Hi folks,
I have set the input and output resolution on the H.264 encoder to 2032x1536. My understanding is that this resolution will not require the MegaPixel encoding element to be enabled.
However, I am still seeing flickering at the right hand side of the image.
Is there a maximum resolution that can be encoded without enabling the MegaPixel encoding element and will not result in flickering at the right hand side of the image?
The H.264 encoder version that I am using is version 2.00.02.02.
Thanks in advance,
Terry