Hi,
I'm using HEVC encoder 2.0.0.0 from this thread: http://e2e.ti.com/support/embedded/multimedia_software_codecs/f/356/t/403601
I'm experiencing the following issues:
1) Looks like HEVC encoder 2.0.0.0 package is not well formed. Unlike other codecs it doesn't link with the library when I do xdc.loadPackage in app.cfg
2) When parameters are incorrect HEVC just fails in algInit with -1. Is there any way to understand what exactly is wrong?
3) HEVC encoder creates 2 barriers with the same name on the same core - one multi DSP and another multi core. It breakes multicore API rules. I created workaround for this but still it looks like a bug that may lead to confusion. Logs:
swbarr name=H265Ebarrier9 user_id=0 num_users=2 user_ids=0,8
swbarr name=H265Ebarrier9 user_id=1 num_users=8 user_ids=0,1,2,3,4,5,6,7
Full logs: 7635.logs.zip
Regards,
Andrey Lisnevich