Hi,
On TI website, I download the following library:
AEC-AER:
Acoustic Echo Cancellation/Removal for TI C64x+, C674x, C55x and Cortex(tm)A8 Processors
I hope to run some simple examples on C5535 eZDSP, but I cannot find any example or documentation on echo cancellation usage. The documents are about fine tune, test etc. topics. Although it does mention The C library and the assembly library
but what API and what functions inside the libraries?
I have searched this topic on the e2e forum, such as the following link:
https://e2e.ti.com/support/embedded/multimedia_software_codecs/f/356/p/119678/433036
it used function: COMMON_create:
aech = (AEC_ITTIAM_Handle)COMMON_create(codecs->eh, "aec", (COMMON_Params*)&AEC_Params);
if (aech == NULL) {
dbg( "Can't create handle for echo canceller\n");
goto error_free ;
}
but I don't see the only example project: aertest_c55l_C55L_COFF using that function.
I do not find it in the
AER Bundle User's Manual
I want to run an echo cancellation function on C5535 eZDSP now. Can anybody help me?
Thanks